Infineon introduces 80 V MOSFET OptiMOS™ 7 with lowest on-resistance in the industry for automotive applications

Mar 27, 2024 | Market News

Munich, Germany – 27 March 2024 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) has introduced the first product in its new advanced power MOSFET technology OptiMOS™ 7 80 V: The IAUCN08S7N013 features a significantly increased power density and is available in the versatile, robust, and high-current SSO8 5 x 6 mm² SMD package. The OptiMOS™ 7 80 V offering is a perfect match for the upcoming 48 V board net applications. It is designed specifically for the high performance, high quality and robustness needed for demanding automotive applications like automotive DC-DC converters in EVs, 48 V motor control, for instance electric power steering (EPS), 48 V battery switches and electric two- and three-wheelers.

Compared to the previous generation, the R DS(on) of the Infineon IAUCN08S7N013 has been reduced by more than 50 percent, and is now the best R DS(on) in the industry with a maximum of 1.3 mΩ. Users benefit from minimized conduction losses, superior switching performance and the highest power density in a 5 x 6 mm² package. In addition, the IAUCN08S7N013 also features low package resistance and inductance, as well as a high avalanche current capability. For automotive applications, it has an extended qualification that goes beyond AEC-Q101.

Availability

The IAUCN08S7N013 is in mass-production and available now. More information is available at www.infineon.com/iaucn08s7n013/.

Infineon at Embedded World

Embedded World will take place in Nuremberg from 9 to 11 April, 2024, Germany. Infineon will present its products and solutions for decarbonization and digitalization in hall 4A, booth #138 and virtually. Company representatives will also hold several TechTalks as well as presentations at the accompanying Embedded World Conference, followed by discussions with the speakers. If you are interested in interviewing an expert at the show, please email media.relations@infineon.com . Industry analysts interested in a briefing can email MarketResearch.Relations@infineon.com . Information about the Embedded World show highlights is available at www.infineon.com/embedded-world.

About Infineon

Infineon Technologies AG is a global semiconductor leader in power systems and IoT. Infineon drives decarbonization and digitalization with its products and solutions. The company has around 58,600 employees worldwide and generated revenue of about €16.3 billion in the 2023 fiscal year (ending 30 September). Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the OTCQX International over-the-counter market (ticker symbol: IFNNY).

Further information is available at www.infineon.com

This press release is available online at www.infineon.com/press

Follow us: X - Facebook - LinkedIn

Information Number

INFATV202403-084

Press Photos

  • Infineon has launched OptiMOS™ 7 80 V, a new advanced power MOSFET technology with increased power density, available in a versatile SSO8 5 x 6 mm² SMD package, ideal for 48 V board net applications in demanding automotive systems like EVs, electric power steering, and battery switches.
    Infineon has launched OptiMOS™ 7 80 V, a new advanced power MOSFET technology with increased power density, available in a versatile SSO8 5 x 6 mm² SMD package, ideal for 48 V board net applications in demanding automotive systems like EVs, electric power steering, and battery switches.
    TDSON-Automotive-OptiMOS7

    JPG | 428 kb | 1152 x 1202 px