Smallest 3D camera worldwide brings Augmented Reality to a smartphone
Munich, Germany, and San Francisco, CA, USA – June 9, 2016 – Lenovo is the first manufacturer worldwide to bring Tango technology to a consumer product. Google's technology that allows devices to understand spatial information is an exclusive feature in the PHAB2 Pro smartphone launched today. Based on the Time-of-Flight principle, the REAL3™ image sensor chip from Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) equips the smartphone with a 3-dimensional perception of the surroundings in real-time. Infineon provides the only image sensor chip worldwide meeting Google’s specifications.
“Through the Tango-enabled PHAB2 Pro, we are opening a completely new era in mobile applications,” said Hua Zhang, Vice President, Lenovo Android/Chrome Computing Business Group. “The REAL3 image sensor chip from Infineon is a key component for Lenovo’s PHAB2 Pro.” Its users have instant access to Augmented Reality, benefiting from the phone’s motion tracking feature which responds to physical movements, depth perception that measures the distance between objects and area learning capability which enables the device to recall the data recorded from previously visited locations.
Augmented Reality for everyone is no longer a dream
“3D machine vision will drive multiple new applications both in the consumer and the automotive world,” said Jochen Hanebeck, President of the Automotive division at Infineon. “The depth perception and motion tracking today implemented in Tango devices can also be applied to driver monitoring or gesture detection inside the car.”
The sensor chip was developed in Graz, Austria, a global Infineon competence center for advanced semiconductor solutions combining analog and digital signal processing with high data rates. It integrates the pixel array, the control circuitry, ADCs and the digital high-speed interface on a single chip. The development was made in co-operation with pmdtechnologies, a worldwide leading provider of the Time-of-Flight (ToF) technology.
This measuring principle involves infrared light. For each of its pixels, the 3D image sensor chip measures the time the light takes to travel from the camera to the object and back again. Each pixel detects the brightness value of the objects. Compared to other technologies, the ToF technology from pmdtechnologies offers the best spatial resolution and highest robustness both mechanically and concerning background light. Yet, it has the lowest current consumption and size. Thus, the camera is currently the smallest 3D-camera worldwide.
Followers of Google’s developer conference, Google I/O, just recently witnessed Infineon’s involvement in Project Soli: Google and Infineon collaborated on a sensor chip facilitating gesture recognition. The Project Soli works with 60 GHz radio microwaves, whereas Tango is based on sending and receiving infra-red light signals. Thus, it stands apart from common 3D imaging methods. These are either based on a stereo camera requiring a minimum distance for triangulation and higher computing efforts. Alternatively, 3D images could so far be created with structured light with a lower object resolution, involving a higher bill of materials.
About Infineon
Infineon Technologies AG is a world leader in semiconductor solutions that make life easier, safer and greener. Microelectronics from Infineon is the key to a better future. In the 2015 fiscal year (ending September 30), the company reported sales of about Euro 5.8 billion with some 35,400 employees worldwide. Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the over-the-counter market OTCQX International Premier (ticker symbol: IFNNY).
Information Number
INFXX201606-064
Press Photos
-
The 3D camera module featured in Lenovo’s new PHAB2 Pro smartphone (left) with Infineon’s REAL3™ image sensor chip, compared in sizeFoto_Kameramodul
JPG | 1.86 mb | 6016 x 4016 px
-
Lenovo’s new PHAB2 Pro smartphone (Photo: Lenovo)Foto_Phab2_Pro_Color_Option_GS
JPG | 576 kb | 2000 x 1126 px
-
Schematic picture of Lenovo’s new PHAB2 Pro smartphone – the 3D camera module is seen above, with the fisheye lens below (Photo: Lenovo)Foto_Phab2_Pro_Exploded_Camera
JPG | 450 kb | 2000 x 1126 px