EV charging
Please choose a subcategory

DC and AC solutions for EV charging
Along with the ever-growing number of electric vehicles on the market and pressure from governments to reduce vehicle emissions to zero latest by 2050, there is a strong need for more efficient charging solutions. As various consumer studies show, the acceptance of electromobility very much depends on the availability and duration of the charging process, high-power DC fast charging stations are an important piece addressing these market requirements. Already today, a typical EV can charge about 80% of its battery capacity in less than 10 minutes. This is comparable to refueling a conventional car with internal combustion engine. In addition to DC fast charging stations there AC EV Charging offers a lower cost alternative when EV users have sufficient time to charge their EV's.
As the market leader in power electronics, Infineon helps you to bring energy-efficient DC fast charging designs and ready-to-use AC EV charging solutions to life. Benefit from one of the most comprehensive, ready-to-implement one-stop product and design portfolios on the market that covers the entire product range from power conversion, microcontrollers, security, auxiliary power supply, and communication.
Infineon’s discrete products offer the best price/performance ratio. These include on the one hand side our products for power conversion like 600 V CoolMOS™ SJ MOSFET P7 and CFD7 families,600 V CoolMOS™ 8, 650 V IGBT TRENCHSTOP™ 5 and 650V/750V/1200 V CoolSiC™ MOSFET. Our CoolMOS™ and CoolSiC™ MOSFETs matchless advantages include high frequency operation, high power density and reduced switching losses. Our portfolio of high voltage switches is complimented by 650 V and 1200 V CoolSiC™ Schottky diodes. Since every switch needs a driver, and every driver needs to be controlled, we also offer the matching EiceDRIVER™ gate driver as well as XMC™ and AURIX™ microcontrollers for EV charging designs. Infineon's portfolio offer as well IGBTs CoolSiC™ MOSFETs and diode power modules, e.g. CoolSiC™ Easy Modules, IGBT EconoPACK™ and the IGBT EconoDUAL™ family. Charger piles with a capacity of more than 100kW are usually built in a modular approach with stacked sub-units. Our products for charge control include Infineon’s AIROC™ Wi-Fi & Bluetooth® combo chips, the PSOC6 microcontrollers, XENSIV™ current sensors, NOR flash memories, CoolSET™ & OPTIGA™ ensuring data protection and security.
Boards & Designs

EVAL_QDPAK_FB_V2_1


DEMO_HV_PACKAGE


EVAL-1EDSIC-PFC-5KW


EVAL-FFXMR20W2M1HX


EVAL-1ED3144MC12H-SIC


EVAL-1ED3145MC12H-SIC


EVAL-1ED3142MC12H-SIC


EVAL-2ED3146MC12L


EVAL-2EP130R-PR-SIC


EVAL-2EP130R-PR


EVAL-2EP130R-VD


REF_3K3W_TP_SIC_TOLL


EVAL-FFXMR20KM1HDR


EVAL-XMC4800PSOC6M5


EVAL-COOLSIC-2KVHCC


EVAL-1ED3142MU12F-SIC


KIT_1EDB_AUX_SIC


EVAL-1ED3321MC12N


REF-DAB11KIZSICSYS


GS-EVM-FB-650V150A-SP1


GS-EVM-HB-650V150A-SP1


GS-EVB-FB-650V150A-SP1A


EVAL-FFXMR12KM1DR

Simulation Models
Discrete IGBT Motor Drive Simulator

CIPOS™ IPM Simulation

Simulate ONLINE - Sensor technology

Simulation Tools

IPOSIM – Infineon power simulation tool


Solution Finder

Simulate ONLINE - Microcontrollers, AURIX™, XMC™, Embedded power devices

MATLAB
- MathWorksPremium Partner
Simulink
- MathWorksPremium Partner
Simscape Electrical
- MathWorksPremium Partner
Development Tools

Simulation Model Finder


Infineon MOSFET Finder


Infineon Gate Driver ICs Finder


Infineon Smart Power Switches Finder


Evaluation Board Finder

Software Development Kit for XMC™ (DAVE™)


ESD Protection Finder


Connected Secure System Finder


Transceiver Finder


Voltage Regulator Finder


Diode Rectifier Finder


IPM Finder


Bipolar Transistor Finder


Bipolar Disc Finder


IGBT Discrete Finder


I-jet Debug probe
- IARPreferred Partner
I-jet provides a fast debugging platform via JTAG and SWD/SWO with download speeds of up to 1,89 MByte/sec and support for SWO speeds of up to 60MHz and supports all Arm Cortex-A/R/M cores.
The JTAG and Serial Wire Debug (SWD) clocks up to 32MHz (no limit on the MCU clock speed).

C-RUN
- IARPreferred Partner
C-RUN performs runtime analysis by checking application execution directly within the development environment.
It checks for arithmetic issues, bounds issues and heap integrity and will tell you what went wrong and where.

IAR Visual State
- IARPreferred Partner
It is used to graphically design state machines (based on UML) and generate C,C++, C# or Java source code.
It is an excellent tool for design tasks dealing with functional safety as functional safety standards, for example the IEC 61508 standard, recommends state machines as one design method to meet higher SIL levels.

IAR Build Tools for Arm, Functional Safety Edition
- IARPreferred Partner
The certification validates the quality of IAR Systems’ entire development processes, as well as the delivered software.
The certified version offers cross-platform support for Linux (Ubuntu and Red Hat) and Windows.
It is based on the build tools in the IAR Embedded Workbench for Arm, functional safety edition.

IAR Embedded Workbench for Arm, Functional Safety Edition
- IARPreferred Partner
The certification validates the quality of IAR Systems’ entire development processes, as well as the delivered software.
The IAR Systems tools are certified according to ten different standards for functional safety.
In addition to the stron technology, IAR Systems dedicated team and long-term safety support services are available for customers.

IAR Build Tools for Arm
- IARPreferred Partner
supporting implementation in cross platform-based frameworks (Ubuntu, Red Hat or Windows) for automated application build and test processes.
Static code analysis is available with the add-on product C-STAT.

IAR Embedded Workbench for Arm
- IARPreferred Partner
The toolchain generates very fast, compact code, and enables developers to take full control of the code.
It offers support for the FM MCU microcontroller family, XMC industrial microcontrollers, the automotive FCR4, Traveo I and Traveo II family.
In addition, the toolchain supports the PSoC 4, PSoC 5LP and PSoC 6 programmable system on chip.

C-STAT
- IARPreferred Partner
C-STAT includes nearly 1000 checks defined by MISRA C:2012, MISRA C++:2008, and MISRA C:2004 and more than 250 checks mapping to issues covered by CWE. It ensures secure CERT C coding and is also available as TÜV SÜD certified version for selected IAR functional safety editions.

I-jet Trace probe
- IARPreferred Partner
The trace data collection can be done with up to 16-bit wide with 350MHz ETM trace clock and 64-bit time stamp with CPU cycle accuracy.
Infinite code coverage and profiling is enabled by the included streaming trace feature.
Embedded Software

IAR Secure Deploy
- IARPreferred Partner
IAR Embedded Trust
- IARPreferred Partner
Embedded software development
- PromwadAssociated Partner
IAR Embedded Secure IP
- IARPreferred Partner
AUTOSAR Blockset
- MathWorksPremium Partner
Motor Control Blockset
- MathWorksPremium Partner
Embedded Coder
- MathWorksPremium Partner
Services
Training InfineonSpice: Desktop simulation tool

Industrial Automation Solutions: Hardware & Software
- PromwadAssociated Partner

EVAL_QDPAK_FB_V2_1


DEMO_HV_PACKAGE


EVAL-1EDSIC-PFC-5KW


EVAL-FFXMR20W2M1HX


EVAL-1ED3144MC12H-SIC


EVAL-1ED3145MC12H-SIC


EVAL-1ED3142MC12H-SIC


EVAL-2ED3146MC12L


EVAL-2EP130R-PR-SIC


EVAL-2EP130R-PR


EVAL-2EP130R-VD


REF_3K3W_TP_SIC_TOLL


EVAL-FFXMR20KM1HDR


EVAL-XMC4800PSOC6M5


EVAL-COOLSIC-2KVHCC


EVAL-1ED3142MU12F-SIC


KIT_1EDB_AUX_SIC


EVAL-1ED3321MC12N


REF-DAB11KIZSICSYS


GS-EVM-FB-650V150A-SP1


GS-EVM-HB-650V150A-SP1


GS-EVB-FB-650V150A-SP1A


EVAL-FFXMR12KM1DR

Discrete IGBT Motor Drive Simulator

CIPOS™ IPM Simulation

Simulate ONLINE - Sensor technology


IPOSIM – Infineon power simulation tool


Solution Finder

Simulate ONLINE - Microcontrollers, AURIX™, XMC™, Embedded power devices

MATLAB
- MathWorksPremium Partner
Simulink
- MathWorksPremium Partner
Simscape Electrical
- MathWorksPremium Partner

Simulation Model Finder


Infineon MOSFET Finder


Infineon Gate Driver ICs Finder


Infineon Smart Power Switches Finder


Evaluation Board Finder

Software Development Kit for XMC™ (DAVE™)


ESD Protection Finder


Connected Secure System Finder


Transceiver Finder


Voltage Regulator Finder


Diode Rectifier Finder


IPM Finder


Bipolar Transistor Finder


Bipolar Disc Finder


IGBT Discrete Finder


I-jet Debug probe
- IARPreferred Partner
I-jet provides a fast debugging platform via JTAG and SWD/SWO with download speeds of up to 1,89 MByte/sec and support for SWO speeds of up to 60MHz and supports all Arm Cortex-A/R/M cores.
The JTAG and Serial Wire Debug (SWD) clocks up to 32MHz (no limit on the MCU clock speed).

C-RUN
- IARPreferred Partner
C-RUN performs runtime analysis by checking application execution directly within the development environment.
It checks for arithmetic issues, bounds issues and heap integrity and will tell you what went wrong and where.

IAR Visual State
- IARPreferred Partner
It is used to graphically design state machines (based on UML) and generate C,C++, C# or Java source code.
It is an excellent tool for design tasks dealing with functional safety as functional safety standards, for example the IEC 61508 standard, recommends state machines as one design method to meet higher SIL levels.

IAR Build Tools for Arm, Functional Safety Edition
- IARPreferred Partner
The certification validates the quality of IAR Systems’ entire development processes, as well as the delivered software.
The certified version offers cross-platform support for Linux (Ubuntu and Red Hat) and Windows.
It is based on the build tools in the IAR Embedded Workbench for Arm, functional safety edition.

IAR Embedded Workbench for Arm, Functional Safety Edition
- IARPreferred Partner
The certification validates the quality of IAR Systems’ entire development processes, as well as the delivered software.
The IAR Systems tools are certified according to ten different standards for functional safety.
In addition to the stron technology, IAR Systems dedicated team and long-term safety support services are available for customers.

IAR Build Tools for Arm
- IARPreferred Partner
supporting implementation in cross platform-based frameworks (Ubuntu, Red Hat or Windows) for automated application build and test processes.
Static code analysis is available with the add-on product C-STAT.

IAR Embedded Workbench for Arm
- IARPreferred Partner
The toolchain generates very fast, compact code, and enables developers to take full control of the code.
It offers support for the FM MCU microcontroller family, XMC industrial microcontrollers, the automotive FCR4, Traveo I and Traveo II family.
In addition, the toolchain supports the PSoC 4, PSoC 5LP and PSoC 6 programmable system on chip.

C-STAT
- IARPreferred Partner
C-STAT includes nearly 1000 checks defined by MISRA C:2012, MISRA C++:2008, and MISRA C:2004 and more than 250 checks mapping to issues covered by CWE. It ensures secure CERT C coding and is also available as TÜV SÜD certified version for selected IAR functional safety editions.

I-jet Trace probe
- IARPreferred Partner
The trace data collection can be done with up to 16-bit wide with 350MHz ETM trace clock and 64-bit time stamp with CPU cycle accuracy.
Infinite code coverage and profiling is enabled by the included streaming trace feature.

IAR Secure Deploy
- IARPreferred Partner
IAR Embedded Trust
- IARPreferred Partner
Embedded software development
- PromwadAssociated Partner
IAR Embedded Secure IP
- IARPreferred Partner
AUTOSAR Blockset
- MathWorksPremium Partner
Motor Control Blockset
- MathWorksPremium Partner
Embedded Coder
- MathWorksPremium Partner
Training InfineonSpice: Desktop simulation tool

Industrial Automation Solutions: Hardware & Software
- PromwadAssociated Partner
Login to myInfineon to see all documents available
-
Infineon EiceDRIVER™ gate driver ICs selection guide
EN
CN
02_00 | 2022-05-04 | pdf | 13 MB
-
Gate Driver ICs for EV-charging stations and wall boxes
EN
02_00 | 2022-02-15 | pdf | 558 KB
-
Next Generation CoolMOS™ based solutions for EV Charging
EN
01_00 | 2020-10-21 | pdf | 1.3 MB
-
600 V CoolMOS™ CFD7
EN
CN
JA
02_01 | 2023-06-06 | pdf | 1.1 MB
-
Linear FET combines advantages of planar and trench MOSFETs
EN
CN
01_00 | 2022-06-09 | pdf | 2.4 MB
-
MOSFET CoolMOS™ CFD7A 650V - for on-board chargers and DC-DC converters
EN
CN
JA
02_00 | 2020-09-01 | pdf | 2 MB
-
MOSFET CoolMOS™ CE optimizing CoolMOS™ CE based power supplies for EMI
EN
CN
JA
01_00 | 2016-11-09 | pdf | 4.8 MB
-
DC EV Charging Solutions Application Brief
EN
01_00 | 2024-09-05 | pdf | 643 KB
-
How to make the charging infrastructure for electric vehicles smart
EN
CN
JA
02_01 | 2022-11-01 | pdf | 781 KB
-
Realizing the future of fast EV charging through CoolSiC™ based topology design
EN
JA
02_01 | 2022-01-01 | pdf | 2.1 MB
-
Implementing Fast DC BEV Chargers up to 150 kW
EN
KO
01_00 | 2019-12-18 | pdf | 605 KB
-
Das breite Einsatzspektrum der CoolSiC™ MOSFET Technologie - elektronik industrie, 12/2019
DE
01_00 | 2019-12-17 | pdf | 482 KB
-
Tackling the Challenges of Electric Vehicles Fast Chargings
EN
JA
01_00 | 2019-12-12 | pdf | 6.5 MB
-
Befeuern der DC- Ladeinfrastruktur - Leistungsbausteine für schnelles Laden
DE
01_00 | 2019-04-25 | pdf | 705 KB
-
Electric Vehicle Fast Charging Challenges
EN
01_00 | 2019-03-20 | pdf | 1.3 MB
-
How long is your system going to last?
EN
01_00 | 2018-12-12 | pdf | 472 KB
-
Charging eTrucks and eBuses (eCAV) vs. charging passenger cars
EN
01_00 | 2025-03-12 | pdf | 4 MB
-
DC EV Charging Application Presentation
EN
01_00 | 2025-02-28 | pdf | 1.5 MB

Our latest whitepaper examines how Vehicle-to-Grid (V2G) technology with smart charging can revolutionize the way we power our world. Learn more about the key benefits and crucial components required to create a truly "smart" charging infrastructure. Additionally, explore how Infineon’s cutting-edge solutions ensure vehicle owners can confidently embrace this technology without concerns over battery degradation.

In this on-demand webinar, our expert will provide a high-level overview of truck and bus charging and its similarities and differences to passenger vehicle charging. In particular, we will discuss the impact that charging, especially in the megawatt range, can have on the selection of power semiconductors and how Infineon is positioned. Recharge your knowledge now.
Watch now
Podcast4 Engineers - DC vs. AC in EV Charging with Torsten Klemmer and Daniel Makus
In this episode, our application managers Torsten Klemmer and Daniel Makus discuss the strengths and weaknesses of both DC and AC charging designs for electric vehicles.
Podcast4 Engineers - Bi-directionality in EV Charging with Daniel Makus
In this podcast episode, our application manager Daniel Makus and host Fabian Schiffer talk about the new opportunities bi-directionality is opening up in EV Charging and other applications.
Podcast4Engineers: Vision for eMobility: 10kWh for 100km with Dirk and Christoph
In this episode, our expert guests Dirk and Christoph explain “10 kWh for 100 km” and discuss how semiconductors not only enable decarbonization in eMobility, but also ensure the “fun-to-drive” factor.
Ask the Expert: AC wallboxes
Charging your EV at home is convenient, but how do you choose a wallbox? In this episode of “Ask the Expert”, our expert Hakan explains what makes AC wallboxes unique.
Ask the Expert: Connectivity in AC wallboxes
Why is it important to keep your AC wallbox connected and secure? In this episode of “Ask the Expert”, our expert Hakan explains how connectivity can make your charging experience more convenient, efficient, and even save you money.
Efficient bidirectional EV charging
Empowering energy independence. Find out more about Infineon's semiconductor solutions for efficient bidirectional EV charging.
CoolSiC™ for automotive applications – Revolution to rely on
With an outstanding quality of robust, large and reliable semiconductor portfolio of automotive CoolSiC™ devices, Infineon is paving the way for carbon-efficient e-mobility.
DC EV charger - The future of electric mobility
DC-Charger are a backbone of current and future electric mobility. Our expert briefly explains the application, the challenges and some of the driving forces behind it. It closes with a hint on how and where to find suitable Infineon-Products easily.
EV charging - General Information
EV charging - Detailed Information
Webinars
Webinar: Charging eCAV vs. charging passenger cars and the impact on power semiconductors
Follow the discussion on the impact of the right selection of power semiconductors, especially in the megawatt range, and how Infineon is positioned.
Introducing the discrete TRENCHSTOP™ IGBT7 family
Driving decarbonization and digitalization together is crucial and the IGBT7 technology plays a major role along this entire energy chain. This training video will introduce the discrete TRENCHSTOP™ IGBT7 family and share its five decisive values and the application positioning.
Introduction to 2EP1xxR EiceDRIVER™ power - Module 2
In the technical introduction training, you became familiar with the full-bridge transformer driver family 2EP, which is a reliable power supply that supports Infineon’s top-notch switches and isolated gate drivers. By the end of this deep dive, you will be able to describe the working principle of this family and know about possible applications by understanding the effect of input voltage changes, transformer transfer ratio, and duty cycle changes on the isolated output voltage.
Introduction to 2EP1xxR EiceDRIVER™ Power - Part 1
This video will introduce you to the 2EP EiceDRIVER™ power family, along with its features and advantages. Additionally, you will have an overview of the extensive application scope of the 2EP.
Fast DC EV charging with CoolSiC™ from Infineon
As electro mobility increasingly becomes part of our daily lives, the need for more efficient charging solutions is growing. With an eye on the requirements and technological developments in this field, the challenge is to respond with smart and compact power conversion solutions for the charging networks of today and tomorrow. In this webinar, you will gain deeper insights, into Infineon's comprehensive DC-EV charging portfolio with a focus on silicon carbide and its important contribution to ultra-fast EV charging.
Speed Up EV Charging Designs with Infineon’s Reference Solutions
The Tech Driving Bi-directional EV Charging
Today's global challenges of decarbonization, combined with rising energy demand, make bi-directional electric vehicle charging and how semiconductor solutions support this application more important than ever. In this webinar you will get an overview of the power conversion topologies for bi-directional DC charging and take a closer look at an application example based on Infineon's 50 kW Reference Design.
AC EV Charging | Market Application Problem Solution System (E1)
The training overviews the different types of chargers with focus on AC EV charging and its functionality, it also positions products from Infineon for the AC chargers with focus on control, connectivity and security. The training shows block diagrams of the difference solutions.
DC EV Charging | Market, Application, Problem, Solution & System (E1)
The training overviews the different types of chargers with focus on DC EV charging and its functionality, it also positions products from Infineon for the DC chargers with focus on control, connectivity and security. The training shows block diagrams of the difference solutions.
Online Courses
Introducing wireless connectivity solutions for DC EV charging
This training provides an overview of the importance of reliable and secure connectivity for EV charging stations, and how Infineon's Wi-Fi 6 solution can help overcome common challenges in EV charging.
Introducing CAN-transceivers and digital isolators for EV charging
This training provides an overview of the fundamentals of internal communication in DC EV charging, including the role of CAN FD and ISOFACE™ digital isolators in enabling reliable and efficient communication between different components of the charging system.
Introducing memory solutions for DC EV charging
As the world shifts to electric vehicles, there are three main demands charging infrastructure must face: efficiency, reliability, and security. Infineon’s memory solutions are designed to address the reliability and security required by the charging systems that can handle the demands of the future.
Main Inverter CoolSiC kit introduction video
In depth introduction of Infineon's one stop shop reference design for EV traction Inverter.
Getting started with the EiceDRIVER™ X3 digital evaluation board

- Understand Infineon’s purpose in delivering quality above and beyond the standard and find out how we execute that standard in development, qualification, manufacturing and testing
- Learn where and how this high-quality standard is reflected and discover our success stories
CoolSiC™ MOSFET in an EV charging application
With the growing market of electrical vehicles, the industry has put forward more requirements for the performance of charging piles. This e-learning will show you that the emergence of CoolSiC™ MOSFETs has improved the charging pile industry to make the EV charger smaller, faster and with higher efficiency.
#ew23 - Tech Talks - 3. Next-generation eMobility.mp4

- Distinguish the features and benefits of Infineon’s CoolSiC™ solutions in target applications and identify Infineon’s fully scalable CoolSiC™ portfolio to meet this automotive market transition
- Explain the reasons for the increasing introduction of silicon carbide technology in the automotive applications
Standards for wireless charging
This training covers the harmonized frame of standards from international bodies like ISO, IEC, SAE and UL dedicated to the Wireless Power Transfer system technologies.

In this online course you will learn about cost-optimized, but highly efficient electric vehicles charging solutions based on IGBT and CoolMOS™, and explore Infineon’s wide portfolio that supports every segment of the EV charging application.

This training covers the most relevant standards for high power charger design, grouped into 4 major areas:
• charging topology
• communication
• accessories
• safety and security

- The training covers detailed information about Infineon's 3rd generation automotive EiceDRIVER™ 1EDI305xAS
- Participants will learn how these products help to reduce switching losses and improve thermal efficiency, resulting in longer range for hybrid and electric vehicles
EiceDRIVER™ isolated gate driver family overview
Every switch needs a driver, and the right driver makes a difference.
Infineon offers different isoalted gate driver families, such as the EiceDRIVER™ Compact and the EiceDRIVER™ Enhanced. Each family has different features to protect the switch and application.
The EiceDRIVER™ isolated gate driver offers advanced features such as reinforced isolation, Miller clamp, slew rate control and short circuit protection to protect the switch and application. It also enables condition monitoring and rapid prototyping.
The EiceDRIVER™ is the perfect fit for industrial application, particular in combination with Infineon CoolSiC™ and IGBT switches.

Training topics:
- Get to know how AURIXTM is able to answer the needs of the electric vehicle market
- Recognize and explore how AURIX™ TC3xx addresses key electric vehicle challenges, and understand the main features of the AURIX™ TC3xx microcontroller

In this training you will:
- Be familiar with silicon carbide MOSFET structures and their characteristics
- Get to know Infineon's CoolSiC™ MOSFET, its features, its improvements over a typical trench MOS and how it performs against its competitors

In this training you will:
- Get to know Infineon’s IPOSIM tool, specifically for an automotive electric vehicle inverter
- Discover the steps involved in simulating different parameters and comparing the results of different Infineon products to see which is the best fit for your application

In this training you will:
- Learn about the transition from fule injection combustion engine to full battery electric vehicles and the main 48V powered applications.
- Additionally get an overview about Infineon’s comprehensive MOSFET portfolio for 48 V applications and their support material

- Infineon's HybridPACK™ Drive silicon carbide compact power modules cater to the increasing demand for high range, efficiency, and power in electrified vehicles, enabling longer drive range, compact size, and optimized system cost.
- The second generation of Infineon's HybridPACK™ Drive, utilizing CoolSiC™ technology, offers a scalable product family with enhanced features and package improvements, providing added value to customers.

- Describe the key features and benefits of Infineon's EiceDRIVER™ isolated gate driver family and explain why it is suitable for the xEV main inverter
- List the target applications of the EiceDRIVER™ gate driver family and recall the reference designs available
Top 6 FAQs. Use the search bar above to show more!
How to get Technical Support?
The best way to reach out to our Applications Engineers is through our Infineon Developer Community
Our Applications Engineers moderate the community to ensure all questions are answered quickly and accurately, either by others in the community or by our own engineers.
If you have any further questions, please submit your request via the Infineon myCases portal. This is a direct channel to get fast and easy support for your needs.
To register, Click on "Register for myInfineon” available at the top right corner of the Infineon homepage and follow the instructions.
To take advantage of additional benefits we recommend to register your corporate email address.
To log-in, click on “Login to myInfineon”.
By clicking on the My Cases link, you will be guided to the My Cases Customer Portal.
You can visit the link directly through: https://mycases.infineon.com.
If any questions, please contact our hotline, https://www.infineon.com/call.
Read more
How to find a Partner to support on SW, HW, dev tools and services?
Infineon’s global network of partners offer products and services that complement our semiconductor device solutions to accelerate your development efforts and time to market. You can find them here: https://www.infineon.com/partnerfinder.
Read more
Where to find the Package information?
The package information is available on our homepage. Please note, that they are divided into the subcategories “Leaded and through-hole”, “Surface Mounted Devices” and “Special Packages”. You will find all relevant package information at the option that applies.
Read more
Where to find board assembly information of Infineon packages?
Information regarding reflow profile, soldering temperature, soldering profile and further processing notes for most of the discrete products are mentioned in the Application Note.
Please visit https://www.infineon.com/packages and refer to the document General Recommendations for Assembly of Infineon Packages.
For TO-packages please refer to these recommendations.
Read more
How to get Design-in support for an application?
We offer design-in support for your application.
You can use our Infineon Solution Finder: https://www.infineon.com/solutionFinder
Here you select the relevant parameters of your application and narrow down your choice according to your requirements.
Read more
Where to find Simulation parameters & SPICE models?
Please visit our Simulation Model Finder on the internet at
https://www.infineon.com/simulation
Please select "Simulation Models (SPICE, S-parameters, SABER)"
If you cannot find your requested model there, please submit your request via the "click to request model" button on the right handed side.
Infineon uses only Spice and Saber models. These are a generally accepted standard that meets all simulation model requirements.
Read more