英飞凌XMC4500工业单片机和全面的开发工具套件现已供货
2012年2月28日,德国纽必堡和纽伦堡讯 — 英飞凌科技股份公司(FSE:IFX / OTCQX:IFNNY)已发布XMC4500系列产品。这是英飞凌推出的首个基于ARM® Cortex™ M4处理器的32位工业单片机产品家族。XMC4500单片机将于2012年5月投入量产。目前,英飞凌正携XMC4500单片机样品,隆重参加在德国纽伦堡举办的“2012年国际嵌入式系统展”。为 该产品锦上添花的是一套可提供全面支持的开发工具:除英飞凌免费提供的DAVE™ 3开发环境之外,还提供了包括编译器、调试器、软件分析和Flash烧录工具等在内的全套工具,以 及知名供应商提供的范围广泛的软件解决方案和咨询服务。XMC4500系列特别适用于电力传动、太阳能逆变器以及工业自动化和楼宇自控等应用。
英飞凌科技股份公司工业与多元市场部负责单片机业务的高级主管Stephan Zizala博士表示,“相比于其他竞争产品,度身定制的XMC4000家族更加贴合工业客户的特定要求:它 提供了高性能外设和全面的开发环境,便于设计人员轻松上手,节省宝贵的时间,并且完全免费。在XMC4500系列的设计过程中,英飞凌充分发挥了30多年来在开发面向工业应用的单片机方面积累的丰富经验。X MC4500拥有专为电机控制而优化的定时器模块以及快速ADC、集成式Delta-sigma解调器、强大而快速的Flash存储器等特性,并且工作温度范围更宽,最高可达125°C。”
同XMC4000家族的所有成员一样,XMC4500系列有助于提高系统能效,可支持大量通信标准,并且降低了软件开发的复杂度。为此,英飞凌免费提供了集成式DAVE 3开发环境。除 基于DAVE应用生成代码之外,DAVE 3开发环境还配备了GNU编译器、调试器和数据可视化工具等。英飞凌还可提供模块化设计应用套件。取决于不同的应用要求,可将最多三个分别用于实现与其他系统的通信、支 持执行器和传感器以及提供人机接口(HMI)功能的卫星板,连接至中央CPU板。
主频为120MHz的中端XMC4500系列
目前,XMC4500系列包含若干个产品型号,这些产品具备不同的工作温度范围(85 °C或125 °C)、Flash存储容量(512 kB到1 MB不等)和封装( LQFP-100、LQFP-144和LFBGA-144)。XMC4500单片机搭载时钟频率为120 MHz的CPU、160 KByte的RAM以及丰富的外设和接口。外 设包括4个12位快速并行模数转换器模块、两个12位数模转换器模块、4个Delta-sigma解调器模块和6个捕捉/比较单元(CCU4和CCU8)。除此之外,还有两个定位接口模块、一 个触控和一个LED矩阵控制模块。通信功能则包括以太网、USB和SD/MMC等接口。此外,还提供了3个CAN节点、6个串行通信通道和一个外部总线接口。
XMC4500的供货和定价情况
现已可在“2012年国际嵌入式系统展”上订购XMC4500系列样品。取决于所选择的CPU工作频率、工作温度范围和封装等,X MC4500单片机的单价在3.90欧元到5.50欧元不等(订货量达一万颗时)。
其他XMC4000家族成员的供货情况
XMC代表“跨市场的单片机”,正如其名,XMC4000家族适于应用在广泛的工业产品中。目前,XMC4000家族包含5个系列。这几个系列主要在内核频率、内存容量、外 设功能以及I/O端口数量等方面各不相同:XMC4500采用了120 MHz CPU(现已可提供样品)、XMC4100和XMC4200采用了80 MHz CPU、XMC4400采用了120 MHz CPU,而采用180 MHz CPU的XMC4700系列则尚在设计阶段。将从2012年第四季度开始提供XMC4400、XMC4200和XMC4100系列的样品。
更多信息
如欲了解关于XMC4500系列和XMC4000家族的更多信息,请访问 www.infineon.com/xmc和2012年1月23日发布的新闻稿。
如欲了解关于为我们提供工具的合作伙伴的信息,请访问 www.infineon.com/xmc-swt
在2012年2月28日至3月1日在德国纽伦堡举办的“2012年国际嵌入式系统展”上,英飞凌将在4号厅142号展台上展出其XMC4500系列和DAVE 3开发环境。关 于英飞凌在本届展会上的其他精彩亮点,请访问www.infineon.com/embeddedworld。
About Infineon
总部位于德国纽必堡的英飞凌科技股份公司,为现代社会的三大科技挑战领域——高能效、移动性和安全性提供半导体和系统解决方案。2011财年(截止到9月30日),公司实现销售额40亿欧元,在 全球拥有约26,000名雇员。英飞凌科技公司的业务遍及全球,在美国苗必达、亚太地区的新加坡和日本东京等地拥有分支机构。英飞凌公司目前在法兰克福股票交易所(股票代码:IFX)和美国柜台交易市场( OTCQX)International Premier(股票代号:IFNNY)挂牌上市。
更多信息请访问 www.infineon.com。
本新闻稿还可在 www.infineon.com/press/上找到。
Information Number
INFATV201202.028
Press Photos
-
The XMC4500 series is the first device in the 32-bit XMC4000 family on to market. It uses the ARM® CortexT-M4 processorXMC4500
JPG | 461 kb | 1800 x 1328 px
-
The modular design kit for the XMC4500 series. Up to three additional application boards - for actuators and sensors (top), for human-machine interface (HMI) functions (right), and for communication with other systems (left) - can be connected to the basic design board with XMC4500 (middle), depending on the respective application requirements.Application_Board_Kits
JPG | 624 kb | 2126 x 1535 px
-
Dr. Stephan Zizala, Senior Director, Industrial and Multimarket Microcontrollers, Infineon Technologies AGZizala_Stephan
JPG | 1.63 mb | 1535 x 2126 px