A safe for sensitive data in the car: Volkswagen relies on TPM from Infineon

2019-1-25 | 市场新闻

Munich, Germany – January 25, 2019 – Volkswagen is one of the first car makers to deploy the OPTIGA™ Trusted Platform Module (TPM) 2.0 from Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) as a security solution for the connected car. The chip is designed to protect the vehicle’s communication with the outside world. For example, when car-sharing users or third-party services such as parcel delivery into a car’s trunk require access. Furthermore, the TPM is suited to secure software updates over the air by the car manufacturer.

TPMs have proven themselves in the computer industry for many years and are now increasingly being used in connected devices in the Internet of Things. Infineon is the first semiconductor manufacturer to offer an automotive-qualified TPM for the connected car. The chip meets international security standards and is certified by independent authorities.

Like a doorkeeper, the TPM particularly protects the vehicle’s external interfaces, for example in the infotainment system or the telematics unit. It checks the identities of senders and recipients of digital data, such as the manufacturer’s backend server. It encrypts and decrypts the data and helps make sure that only data the driver or manufacturer actually wants makes its way into the car.

The cryptographic keys needed for these security functions are stored within the TPM as in a safe. Infineon imports the initial keys in a specially certified security environment. Since all other keys can be generated, used and stored within the TPM itself, they never have to leave it and are protected against being spied on via the network. The TPM is also hardened against physical attacks. Even if someone removes the chip from the vehicle, the keys are well protected from being read. 

The OPTIGA TPM 2.0 is also designed to accommodate the long product life cycles of cars. Its firmware, including cryptographic mechanisms (“crypto-agility”), can be updated remotely making sure that its security technology is always state-of-the-art.

Infineon has decades of experience in automotive electronics and hardware-based security. With the new OPTIGA TPM 2.0 and its AURIX™ family of microcontrollers, Infineon provides a comprehensive portfolio of application-specific security solutions that address key challenges in the automotive industry.

Further information is available at www.infineon.com/Auto-TPM.

Information Number

INFATV201901-030

Press Photos

  • The new OPTIGA TPM 2.0 SLI 9670 from Infineon is a plug & play solution for automotive applications. It is especially suited for use in a central gateway, the telematics unit or the infotainment system of the vehicle. The SLI 9670 consists of an attack-resistant security chip and high-performance firmware developed in accordance with the latest security standard.
    The new OPTIGA TPM 2.0 SLI 9670 from Infineon is a plug & play solution for automotive applications. It is especially suited for use in a central gateway, the telematics unit or the infotainment system of the vehicle. The SLI 9670 consists of an attack-resistant security chip and high-performance firmware developed in accordance with the latest security standard.
    SLI_9670_VQFN-32-13

    JPG | 309 kb | 2126 x 1546 px

  • Infineon is the first semiconductor manufacturer to offer a Trusted Platform Module specifically for cars. It is suited to secure the vehicle’s communication with the outside world – for example for software updates over the air.
    Infineon is the first semiconductor manufacturer to offer a Trusted Platform Module specifically for cars. It is suited to secure the vehicle’s communication with the outside world – for example for software updates over the air.
    OPTIGA_TPM_2-0

    JPG | 373 kb | 1920 x 1080 px