Two EasyPACK™ modules with CoolSiC™ MOSFETs for EV charging and UPS

2019-9-3 | 市场新闻

Munich, Germany – 3 September 2019 – Production numbers of electric vehicles (full and hybrid) are rapidly increasing. With that, the demand for energy efficient charging solutions is also rising. Addressing the fast growing demand for Silicon Carbide (SiC) solutions in this field, Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) launched two new EasyPACK modules of the 1200 V family. Both, Easy 1B and Easy 2B, integrate CoolSiC™ MOSFETs aiming not only at this market but also at UPS applications.

Coming in two different topologies the power modules enable engineers to increase their systems’ efficiency for reduced cooling effort. In addition, higher frequency operation is possible. Integrated in an Easy 1B housing the four-pack topology (F4-23MR12W1M1_B11) perfectly serves the DC/DC stage of the charging station. The Easy 2B (F3L15MR12W2M1_B69) holds a three-level configuration that is well suited for the Vienna Rectifier usually implemented in this application for the PFC stage. In combination, the power modules can be used for 50/60 kW EV charging solution.

The EasyPACK standard package for power modules is characterized by an industry-leading low stray inductance. This helps in building up stacked modular solutions for charging which can go up to 120/150 kW. The NTC temperature sensor, which is also featured in the Easy modules, facilitates the monitoring of the device, while the PressFIT technology reduces assembly time for mounting the device.

Availability

Both Easy CoolSiC MOSFETs can be ordered now. More information is available at www.infineon.com/coolsic-mosfet.

Information Number

INFIPC201909.096

Press Photos

  • The Easy 1B housing integrates a four-pack topology which perfectly serves the DC/DC stage of an EV charging station. The power modules can be used for charging solutions of up to 50/60 kW or stacked modular solutions of up to 120/150 kW.
    The Easy 1B housing integrates a four-pack topology which perfectly serves the DC/DC stage of an EV charging station. The power modules can be used for charging solutions of up to 50/60 kW or stacked modular solutions of up to 120/150 kW.
    CoolSiC_MOSFET_Easy_1B

    JPG | 161 kb | 1500 x 886 px

  • The Easy 2B holds a three-level configuration that is well suited for the Vienna Rectifier usually implemented for the PFC stage in an EV charging solution. The power modules can be used for charging solutions of up to 50/60 kW or stacked modular solutions of up to 120/150 kW.
    The Easy 2B holds a three-level configuration that is well suited for the Vienna Rectifier usually implemented for the PFC stage in an EV charging solution. The power modules can be used for charging solutions of up to 50/60 kW or stacked modular solutions of up to 120/150 kW.
    CoolSiC_MOSFET_Easy_2B

    JPG | 218 kb | 1500 x 1007 px