New environmental sensor technology: photoacoustic spectroscopy (PAS) miniaturizes CO2 sensor XENSIV™ PAS CO2
Munich, Germany – 18 June 2019 – City dwellers often spend a large amount of their time indoors, either in an office, at school, or simply at home. Urbanized spaces, however, tend to trap and develop bad air quality as they get more insulated for energy efficiency purposes. The concentration of CO 2 is an indicator for bad air quality. Today´s market solutions for monitoring this odorless and colorless gas are bulky and costly or simply not good enough for a widespread adoption. Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) has developed a disruptive CO 2 sensor technology based on the photoacoustic spectroscopy (PAS).
XENSIV™ PAS CO2 makes use of this new technology. It implements a high sensitivity MEMS microphone as a detector and enables significant miniaturization of CO 2 sensors. For this reason, it is ideal for smart home applications and building automation i.e. demand controlled ventilation, as well as various indoor air quality IoT devices such as air purifiers, thermostats, weather stations, and personal assistants. The sensor helps to improve the indoor air quality in a timely and energy efficient manner. Based on an extensive portfolio of patents around the PAS technology, PAS CO2 will not only enable high volume and cost sensitive CO 2 sensing applications but will also pave the road for the detection of other gases in the future.
On a single PCB, the CO 2 sensor integrates the photoacoustic transducer including the detector, the infrared source and the optical filter. It also holds a microcontroller for signal processing and algorithms as well as a MOSFET to drive an infrared source. All the components are developed and designed in-house according to Infineon´s high quality standards, leading to the best-in-class price/performance. For instance, XENSIV PAS CO2 uses the high SNR (Signal-to-Noise Ratio) MEMS microphone XENSIVE IM69D130 as a detector. The sensor thus benefits from Infineon´s long record of accomplishments in acoustic technology and related applications.
PAS CO2 is a real CO 2 sensor in an unprecedented small form factor, enabled by the unique PAS detection principle. The sensor saves more than 75 percent space in customer end products compared to commercially available real CO 2 sensors. Its direct ppm readings, surface mounting capability and simple design allow for an easy and fast integration in low and high volume applications alike.
The integrated microcontroller converts the MEMS microphone output into a ppm reading, which is available either via the serial I²C, UART or PWM interface. XENSIV PAS CO2 CO 2 measurement capabilities cover a range from 0 ppm to 10,000 ppm with an accuracy of ± 30 ppm or ±3 percent of the reading. In a pulsed mode, the XENSIV PAS CO2 CO 2 sensor is designed to have a lifetime of ten years.
Availability
The XENSIV PAS CO2 CO 2 sensor will be showcased at Sensor+Test in Nuremberg and at Sensors Expo in San Jose (California), USA. Early samples are being validated in selected targeted applications. Engineering samples are planned to be available in the first half of 2020, Infineon aims at starting the production in the second half of the same year. More information is available at www.infineon.com/PASCO2.
Infineon at the Sensor+Test 2019 and Sensors Expo 2019
At the Sensor+Test 2019 and the Sensors Expo 2019 trade fair (both from 25 to 27 June 2019) Infineon shows its latest sensor solutions for smart vehicles, the smart home, smart industry and robotics as well as health and fitness applications. Infineon’s demos are presented at booth 429 in hall 1 at Sensor+Test, and at booth 1110 at Sensors Expo. Further information about Infineon at the trade fair is available at www.infineon.com/sensortest and www.infineon.com/sensorsexpo.
Information Number
INFPMM201906-080
Press Photos
-
XENSIV™ PAS CO2 is a real CO2 sensor in an unprecedented small form factor, enabled by the unique PAS detection principle. The sensor saves more than 75 percent space in customer end products compared to commercially available real CO2 sensors. Its direct ppm readings, surface mounting capability and simple design allow for an easy and fast integration in low and high volume applications alike.PAS210_Top
JPG | 314 kb | 1609 x 1535 px