AURIX™ TC4x microcontrollers for embedded AI application development receive safety assessment from Fraunhofer IKS

2024-4-10 | 市场新闻

Munich, Germany – 10 April 2024 – In the automotive industry, embedded AI is becoming increasingly important for safety-critical real-time applications. However, this also creates new requirements and standards that must be considered during the complete product lifecycle. Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) addresses these new requirements with the AURIX™ TC4x microcontroller (MCU) family, which meets the AI-specific safety requirements to achieve SAFE AI compliance, as proposed by the Fraunhofer Institute for Cognitive Systems IKS. The MCUs, with their ASIL-D compliant AI-accelerator (PPU), provide an innovative platform for developing embedded AI-based use cases and automotive applications such as motor control, battery management systems, vehicle motion control and siren detection.

The SAFE AI framework based on ISO PAS 8800 and current state-of-the-art AI regulations is an evaluation methodology developed by Fraunhofer IKS that assesses the trustworthiness of AI in terms of robustness, data utility, operational design domain (ODD) and environmental conditions. The functional safety measures of the AURIX TC4x family thus provides mechanisms for compliance with AI regulations and standards at the application level. By using the AURIX TC4x family, car manufacturers can assess the safety and reliability of AI solutions and identify potential vulnerabilities during system development and operation. For safety-critical real-time applications, the use of AI models like neural networks increases accuracy and provides additional safety in conjunction with the existing physical sensor.

“The integration of safe and reliable AI functionality into automotive microcontroller families is essential to further improve vehicle performance, safety, and comfort,” said Thomas Boehm, Senior Vice President Microcontroller at Infineon. "We are therefore very proud that our AURIX TC4x microcontroller has successfully passed the SAFE AI assessment by the Fraunhofer Institute for Cognitive Intelligence. This underlines our position as one of the leading innovation drivers in the industry.”

More Information

Further information about the SAFE AI Framework is available here: https://www.iks.fraunhofer.de/en/research/safety-assurance.html; More information about the AURIX TC4x microcontroller is available here: https://www.infineon.com/cms/en/product/microcontroller/32-bit-tricore-microcontroller/32-bit-tricore-aurix-tc4x/

Infineon at embedded world

embedded world will take place in Nuremberg, Germany, from 9 to 11 April, 2024. Infineon will present its products and solutions for decarbonization and digitalization in hall 4A, booth #138 and virtually. Company representatives will also hold several TechTalks as well as presentations at the accompanying embedded world Conference, followed by discussions with the speakers. If you are interested in interviewing an expert at the show, please email media.relations@infineon.com . Industry analysts interested in a briefing can email MarketResearch.Relations@infineon.com . Information about the embedded world show highlights is available at www.infineon.com/embedded-world.

About Infineon

Infineon Technologies AG is a global semiconductor leader in power systems and IoT. Infineon drives decarbonization and digitalization with its products and solutions. The company has around 58,600 employees worldwide and generated revenue of about €16.3 billion in the 2023 fiscal year (ending 30 September). Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the OTCQX International over-the-counter market (ticker symbol: IFNNY).

Follow us: X - Facebook - LinkedIn

Information Number

INFATV202404-093

Press Photos

  • Infineon addresses new embedded AI requirements with the AURIX™ TC4x microcontroller (MCU) family, which meets the AI-specific safety requirements to achieve SAFE AI compliance, as proposed by the Fraunhofer Institute for Cognitive Systems IKS.
    Infineon addresses new embedded AI requirements with the AURIX™ TC4x microcontroller (MCU) family, which meets the AI-specific safety requirements to achieve SAFE AI compliance, as proposed by the Fraunhofer Institute for Cognitive Systems IKS.
    Infineon_AURIX_TC4x

    JPG | 191 kb | 2126 x 1752 px