Easy Switch from 8-bit to 32-bit with XMC1000 Industrial Microcontroller Family of Infineon; Samples and Tools Now Available

2013-2-26 | 市场新闻

Neubiberg and Nuremberg, Germany – February 26, 2013 – At the Embedded World Exhibition & Conference 2013, Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) today presented samples of its new XMC1000 industrial 32-bit microcontroller family which provides system designers with strong incentive to switch from 8 to 32 bit MCU architecture. With XMC1000, Infineon offers a fully-featured 32-bit alternative for hitherto 8-bit users by combining the ARM® Cortex™-M0 processor core with powerful peripherals, high productivity design tools and costs typical of 8-bit devices based on production using state-of-the-art, 65nm embedded Flash technology on 300mm wafers. With 32-bit performance at 8-bit cost, the XMC1000 family addresses sensor and actuator applications, LED lighting, digital power conversion, such as uninterruptible power supplies, and simple motor drives, such as those used in household appliances, pumps, fans and e-bikes.

“Design of the XMC1000 family started with a deep understanding of the system requirements of 8-bit industrial applications. By aligning the product architecture and peripherals towards the requirements of applications typcally addressed by 8-bit MCUs, developers can use XMC1000 devices to design a better product in a cost-effective way and bring it to market faster,” says Dr. Stephan Zizala, Senior Director, Industrial and Multimarket Microcontrollers at Infineon Technologies AG. “ XMC1000 creates a decisive incentive for switching architecture from 8 to 32 bit, with its combination of 32-bit performance at 8-bit prices and the user-friendly, free DAVE development environment.”

Development tools for the XMC1000 family comprise the free DAVE™ development platform of Infineon, boot kits and comprehensive applications kits for LEDs, touch panels and energy efficient motor controls. Numerous development partners also offer compilers, debuggers, software analysis tools and flash programmers, as well as embedded software solutions, training and technical support for the XMC1000 family.

The XMC1000 family: 8-bit price for 32-bit performance

The XMC1000 family includes three series: XMC1100 (Entry series), XMC1200 (Feature series) and XMC1300 (Control series). The three series differ essentially in terms of their memory capacity and peripheral set.

XMC1000 MCUs feature 8KB to 200KB flash memory, high-performance PWM timers, 12-bit A/D converters and programmable serial communication interfaces. Different members of the family offer dedicated peripherals, including a module for touch control and LED displays, a peripheral unit for the dimming and color control of LEDs (Brightness and Color Control Unit, BCCU) and a mathematical coprocessor for motor drive controls. The XMC1000 microcontrollers satisfy the requirements defined by the standard IEC60730 Class B, which is prescribed for the safety of household appliances sold in Europe, and offer, for example, hardware error correction (ECC) and corresponding memory tests. A further unique feature is a flash loader with a 128-bit AES accelerator, which allows a developer’ s valuable software IP – particularly important in cost-sensitive applications – to be better protected.

Simple, rapid development with DAVE™

Infineon’s DAVE is a free, graphically-driven development environment that reduces development complexity while taking full advantage of all XMC1000 capabilities. Using pre-configured DAVE Apps, developers benefit from application-specific software components that help to drastically reduce the software development time for microcontrollers. DAVE also eases transition between the Infineon XMC1000 (ARM® Cortex™-M0) and XMC4000 (ARM® Cortex™-M4) microcontroller families. The platform incorporates a free GNU compiler and debugger. To provide additional flexibility to design engineers, Infineon collaborates with numerous development partners, who offer compilers, debuggers, software analysis and flash programmers in addition to embedded software solutions, training and technical support for the XMC1000 family.

Availability of XMC1100, XMC1200, XMC1300 and development kits

The XMC1000 family currently comprises 23 products in TSSOP packages with 16, 28 and 38 pins. Samples of all three XMC1000 series and the DAVE development environment for XMC1000 will be available from March 2013. Volume production is planned for Q4 2013. Depending on the particular XMC1000 series and peripheral set, prices for order quantities of several million units can range between Euro 0.25 and Euro 1.25.

For easy and cost-effective evaluation there are boot kits available for all XMC1000 series, as well as comprehensive application kits for LED, touch panel and motor drive applications. The XMC1100 boot kit for Arduino™ can be amended by Arduino™ Shields allowing the use of a large number of add-on boards for a huge range of applications.

Further information

Further information on the products of the XMC1000 and XMC4000 families is available at www.infineon.com/xmc1000 and www.infineon.com/xmc4000. DAVE is available as a free download from the Infineon website at www.infineon.com/dave.

Infineon will be presenting the new XMC1000 microcontroller family at the Embedded World trade fair (February 26-28, 2013, Nuremberg, Germany) in Hall 4A, Booth 222. Further information at www.infineon.com/embeddedworld.

About Infineon

Infineon Technologies AG, Neubiberg, Germany, offers semiconductor and system solutions addressing three central challenges to modern society: energy efficiency, mobility, and security. In the 2012 fiscal year (ending September 30), the Company reported sales of Euro 3.9 billion with close to 26,700 employees worldwide. Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the over-the-counter market OTCQX International Premier (ticker symbol: IFNNY).

Information Number

INFATV201302-027

Press Photos

  • Dr. Stephan Zizala, Senior Director, Industrial and Multimarket Microcontrollers, Infineon Technologies AG
    Dr. Stephan Zizala, Senior Director, Industrial and Multimarket Microcontrollers, Infineon Technologies AG
    Stephan_Zizala

    JPG | 1.63 mb | 1535 x 2126 px

  • The 32-bit microcontroller family XMC1000 for low-end industrial applications offers 32-bit power for 8-bit prices. It addresses sensor and actuator applications, LED lighting, digital power conversion, such as uninterruptible power supplies, and simple motor drives, such as those used in household appliances, pumps, fans and e-bikes.
    The 32-bit microcontroller family XMC1000 for low-end industrial applications offers 32-bit power for 8-bit prices. It addresses sensor and actuator applications, LED lighting, digital power conversion, such as uninterruptible power supplies, and simple motor drives, such as those used in household appliances, pumps, fans and e-bikes.
    XMC1000_Microcontroller_Family

    JPG | 1.44 mb | 1535 x 2126 px

  • The 32-bit microcontroller family XMC1000 for low-end industrial applications offers 32-bit power for 8-bit prices. Samples of all XMC1000 series and the DAVE development environment for XMC1000 will be available from March 2013.
    The 32-bit microcontroller family XMC1000 for low-end industrial applications offers 32-bit power for 8-bit prices. Samples of all XMC1000 series and the DAVE development environment for XMC1000 will be available from March 2013.
    XMC1000_All Packages_Plain

    JPG | 297 kb | 2067 x 1481 px

  • Infineon is launching the XMC1000 family in three series at the same time: XMC1100 (Entry series), XMC1200 (Feature series) and XMC1300 (Control series). The three series differ essentially in terms of their memory capacity and peripheral set.
    Infineon is launching the XMC1000 family in three series at the same time: XMC1100 (Entry series), XMC1200 (Feature series) and XMC1300 (Control series). The three series differ essentially in terms of their memory capacity and peripheral set.
    XMC1000_Table_Overview

    JPG | 607 kb | 3309 x 2433 px

  • The 32-bit microcontroller family XMC1000 for low-end industrial applications offers 32-bit power for 8-bit prices.
    The 32-bit microcontroller family XMC1000 for low-end industrial applications offers 32-bit power for 8-bit prices.
    XMC1000_Block_Diagram

    JPG | 221 kb | 1654 x 1299 px