Sharing your own car via an app: Infineon and XAIN to collaborate on bringing blockchain into the car

2018-10-25 | 商业及财经媒体

Munich, Germany – 25 October 2018 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) and XAIN have agreed to work together on bringing blockchain technology into the car. The Munich semiconductor maker and the Berlin-based start-up have signed a corresponding Memorandum of Understanding at Infineon’s 1st Automotive Cybersecurity Forum, taking place today in Munich. The goal of the collaboration is to test possible applications and develop suitable ones to market maturity. A first demonstrator shows how access rights, e.g. for car sharing, can be granted decentrally with a smartphone app.

“Cybersecurity is crucial for the data-driven mobility of the future”, says Peter Schiefer, President of Infineon’s Automotive Division. “Blockchain technology has enormous potential in this regard, but its use requires a high degree of coordination between the selected blockchain methodology and the security hardware installed in the car itself. We will be working together with XAIN to achieve this level of configuration.”

A blockchain is a decentralized database that enables speedy transactions and particularly secure, tamper-free storage. In connection with cars, feasible applications for this technology include automated payments, keyless access for car sharing schemes, on-demand services, tuning protection and automated driving functions. Essentially, it is all about the granting of access rights – to the car itself or to specific data in the vehicle. An example involving specific data is when insurance companies offer low rates for car owners with good driving habits.

All of Infineon’s 2 nd generation AURIX™ microcontrollers can provide support for blockchain functionality in cars already today. This support is based on an embedded hardware security module (HSM) that complies with the highest level of the EVITA security standard. An HSM consists of special computing and storage units within the microcontroller. It performs the cryptographic operations and is protected by a dedicated firewall of its own. The 2 nd generation AURIX microcontrollers thus have a secured memory for the digital key used for identification in the blockchain and are able to perform blockchain operations, such as hashing or digital signing, swiftly and securely. Certified security controllers such as the OPTIGA™ TPM 2.0 from Infineon for automotive applications allow even higher security levels to be reached.

However, the creation of new data blocks still represents a challenge for the conventional microcontrollers used in cars. Due to the enormous amounts of required computing power, the so-called mining as used in the context of cryptocurrencies, up to this point in time has been executed by high-performance processors. XAIN, however, is working on a new process that can also be performed on devices that need to be economical in their use of energy – such as microcontrollers in cars.

“We aim to turn cars into fully-fledged network participants”, says Leif-Nissen Lundbæk, founder and CEO of XAIN AG. “As well as being important for offline and real-time capabilities, this also enables a particularly high level of privacy protection in connection with AI technologies. It ensures that private data for machine learning is kept exclusively in local storage. The goal of our collaboration with Infineon is to advance the use of XAIN’s AI technology in cars.” 

At the Infineon Automotive Cybersecurity Forum, Infineon and XAIN are presenting their first demonstrator. It shows how access rights can be granted decentrally, swiftly and securely by means of a smartphone app. An application for this would be a car sharing scheme without a platform or back-office in which all participants are able to spontaneously share their cars with others. The Infineon Automotive Cybersecurity Forum is the first industry conference staged by Infineon at which automotive companies, suppliers and academics have come together to discuss cybersecurity in vehicles.

About Blockchain

A blockchain is a decentralized database that enables speedy transactions and particularly secure, tamper-free storage. It stores the transactions in data blocks. The blocks are chained together in chronological order, each block containing a reference to the previous block. Any attempts to tamper with a block of stored data are easily detectable through the subsequent blocks. The fact that the blockchain is stored decentrally at many different locations simultaneously affords further protection against tampering – new blocks can always be checked by several other participants.

About XAIN

XAIN began as a University of Oxford research project in 2014. The visionary goal of this project was to develop a protocol that would allow humans and machines to collaborate with distributed, energy-efficient, and privacy-protecting intelligent systems. In cooperation with a large number of OEMs and global players – such as Porsche, Daimler and SAP – XAIN is striving to implement its vision with a range of AI products. Applications include the automatic granting of access rights in machines (including production machines and vehicles) and the automation of internal processes by means of a software development kit instead of a cloud platform to enable the best possible privacy protection. In addition, XAIN has created a programming language called FROST for the development of distributed and secure access rights, known as smart policies. These policies can also be directly embedded in hardware – in AURIX microcontrollers, for example.

Further information is available at www.xain.io

About Infineon

Infineon Technologies AG is a world leader in semiconductor solutions that make life easier, safer and greener. Microelectronics from Infineon is the key to a better future. In the 2017 fiscal year (ending 30 September), the Company reported sales of around €7.1 billion with about 37,500 employees worldwide. Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the over-the-counter market OTCQX International Premier (ticker symbol: IFNNY).

Follow us: Twitter - Facebook - LinkedIn

Information Number

INFATV201810-005

Press Photos

  • Dr. Leif-Nissen Lundbæk (left), CEO of XAIN AG, and Peter Schiefer, President of the Division Automotive at Infineon Technologies AG, at the Infineon Automotive Cybersecurity Forum in Munich.
    Dr. Leif-Nissen Lundbæk (left), CEO of XAIN AG, and Peter Schiefer, President of the Division Automotive at Infineon Technologies AG, at the Infineon Automotive Cybersecurity Forum in Munich.
    Infineon_XAIN_01

    JPG | 728 kb | 2126 x 1636 px

  • Infineon and XAIN team up to bring blockchain technology into the car. A first jointly developed demonstrator shows how access rights can be granted decentrally by means of a smartphone app, for example for car sharing schemes.
    Infineon and XAIN team up to bring blockchain technology into the car. A first jointly developed demonstrator shows how access rights can be granted decentrally by means of a smartphone app, for example for car sharing schemes.
    Infineon_XAIN_02

    JPG | 604 kb | 2126 x 1417 px