European research project Power2Power for more efficient power semiconductors launches in Dresden

2019-6-5 | 商业及财经媒体

Dresden, 5 June 2019 – The European cooperation project Power2Power has started. Over the coming three years, 43 partners from eight countries will research and develop innovative power semiconductors with more power density and energy efficiency. Power semiconductors are needed in all stages of energy conversion: generation, transmission, and use. More efficient semiconductors make a major contribution towards reducing carbon dioxide emissions in spite of the world's growing energy needs. Universities, research institutes, small and medium-sized companies and international corporations are involved in this cooperation. Infineon Technologies Dresden GmbH & Co. KG is coordinating this project.

“Collaboration across different levels of the supply chain is a basis for the success of the European microelectronics industry,” said Dr. Reinhard Ploss, CEO of Infineon Technologies AG. “We are also pursuing this approach in the Power2Power cooperation project. In collaboration with our partners, we will be working on new power semiconductors and system architectures with higher energy efficiency. Our goal is: more power from less energy.”

The volume of the Power2Power project will be approximately €74 million. Two thirds of this will be allotted to the German partners. The European Union is funding the cooperation within the scope of the ECSEL (Electronic Components and Systems for European Leadership) program. Funding from Germany will be provided by the Federal Ministry of Education and Research and from the two states of Saxony and Thuringia. The partners from the other seven countries are also being sponsored by their national authorities.

“Saxony is the largest microelectronics cluster in Europe,” stresses Minister-President Michael Kretschmer. European cooperation, such as Power2Power, is enormously important for the continued development of Silicon Saxony. The project takes into account all stages of the supply chain and combines innovation with energy efficiency. This could make a significant contribution towards increasing the competitiveness of the European microelectronics industry. This is one of the reasons why the Free State of Saxony welcomes and supports this research project.” Dr. Herbert Zeisel, undersecretary in the German Federal Ministry of Education and Research (BMBF), emphasizes that, on the whole, the Saxon electronics cluster is an outstanding pillar for European high-tech: “Microelectronics is a key for successful industrial products from Germany and Europe. The latest trade disputes illustrate how sovereignty and autonomy are dependent on a country's own capabilities in research and development. Power2Power shows how we can assert ourselves in the global competition. Europe, Germany, Saxony, and Thuringia are acting in concert in the ECSEL program. In the negotiations in Brussels, the BMBF will advocate for the successful ECSEL program to be continued and administration simplified after 2020.”

The European semiconductor industry employs several hundred thousand people. But in its technology-related user industry, it has a much greater leverage effect. “An important focus is the booming market for power electronics,” says Bert De Colvenaer, Executive Director ECSEL Joint Undertaking. “With regard to the global competition – especially from Asia – Power2Power will help increase the manufacturing share of European companies on the world market and further strengthen its leading positions.”

In Germany in particular, the Power2Power project will help extend the competitiveness of semiconductor production. The supply chain for power semiconductors is especially extensive, which is also evident in this this project: from special silicon wafers (Siltronic), to IGBT production at Infineon in Dresden and subsequent module production at Infineon in Warstein, to systems and the associated knowledge, for example from the SMEs EAAT and AVL and from Dresden University of Technology.

An overview of all the partners in the project can be found at www.infineon.com/power2power.

On several supply chain levels, the Power2Power partners will develop pilot lines at German sites to produce innovative power electronics that are fit for the future. With strong partnerships and investments in innovation, the cooperation project will secure and create highly qualified jobs. Consequently, Power2Power is supporting the Federal Government's High-Tech Strategy 2025.

About Infineon

Infineon Technologies AG is a world leader in semiconductor solutions that make life easier, safer and greener. Microelectronics from Infineon is the key to a better future. In the 2018 fiscal year (ending September 30), the company reported sales of 7.6 billion euros with around 40,100 employees worldwide. Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the over-the-counter market OTCQX International Premier (ticker symbol: IFNNY).

Follow us: Twitter - Facebook - LinkedIn

Information Number

INFXX201906-075

Press Photos

  • 300mm thin wafers from Infineon for the production of very energy-efficient power semiconductors
    300mm thin wafers from Infineon for the production of very energy-efficient power semiconductors
    300mm-Duennwafer

    JPG | 568 kb | 2126 x 1417 px

  • Power electronics made in Europe: Infineon's Hybridpack2™ enables energy-efficient control of motor power in electric vehicles
    Power electronics made in Europe: Infineon's Hybridpack2™ enables energy-efficient control of motor power in electric vehicles
    HybridPACK2_opened

    JPG | 746 kb | 2126 x 1595 px

  • Logo Power2Power
    Logo Power2Power
    Power2Power_Logo

    JPG | 158 kb | 2126 x 1063 px