Infineon Introduces Industry's First OC-768 Silicon Germanium-based MUX/DEMUX Chipset at Supercomm to Take the Lead in the 40G SONET/SDH Market
Atlanta, June 4, 2001 Infineon Technologies (FSE/NYSE: IFX), a leading supplier of communications and fiber optics IC solutions, today announced at Supercomm the industrys first OC-768 (40 Gbit/s) multiplexer/demultiplexer (MUX/DEMUX) chipset for next generation synchronous optical networking/synchronous digital hierarchy (SONET/SDH) communication systems. The new chipset forms a core part of the companys complete end-to-end line card solution for OC-768, and will enable makers of high-speed transmission systems to quickly implement emerging applications such as metropolitan area networks (MAN) at a competitive price.
The optical networking market is expected to boom in the next four years with the OC-768 segment leapfrogging all other high speed transmission technologies, said Christian Winkelmeyr, vice president of Infineons communications group and general manager of the high-speed communications business unit. Along with the OC-768 SONET/SDH framing/mapping expertise, pointer processing and STS-1 granularity technology recently acquired from Catamaran, the chipset announced today is a key component of Infineons total solution for 40Gbit/s communication systems.
Fabricated in the companys market leading Silicon Germanium process, Infineons OC-768 MUX/DEMUX chipset also provides lower power consumption and larger scale integration than existing Gallium Arsenide and Indium Phosphide technologies.
The increasing demand for Internet and multimedia data is set to galvanize telecommunications carriers to deploy OC-768 transmission technologies that require vastly improved performance from ICs. According to Gartner Dataquest (Fiber Optic Food Chain, March 2001), the annual worldwide market for semiconductors used in fiber optic modules and physical layer ICs used for fiber optic communications is expected to reach US$11.7 billion in 2004.
Infineons multiplexer and demultiplexer are highly integrated circuits with 16 times 2.5 Gbit/s input channels multiplexed to a single serial 40 Gbit/s output data stream and vice-versa. The supported data-rates range from 39.8 Gbit/s up to 43 Gbit/s enabling out-of-band Forward Error Correction. The interfaces use Current Mode Logic, and both DC and AC coupling is supported. A 622 MHz and 2.5 GHz reference clock is provided and a Voltage Controlled Oscillator integrated onto each chip.
The multiplexer features Clock Management Unit functionality as well as a selectable 20 GHz and 40 GHz clock output to support both No Return to Zero and Return to Zero line coding, respectively. The demultiplexer integrates Clock and Data Recovery functionality with extremely high input sensitivity of 50mV. Both chips operate at a single 5.5V supply voltage.
The FOA4400 multiplexer chip and the FOA5400 demultiplexer chip as well as evaluation boards are now available.
The optical networking market is expected to boom in the next four years with the OC-768 segment leapfrogging all other high speed transmission technologies, said Christian Winkelmeyr, vice president of Infineons communications group and general manager of the high-speed communications business unit. Along with the OC-768 SONET/SDH framing/mapping expertise, pointer processing and STS-1 granularity technology recently acquired from Catamaran, the chipset announced today is a key component of Infineons total solution for 40Gbit/s communication systems.
Fabricated in the companys market leading Silicon Germanium process, Infineons OC-768 MUX/DEMUX chipset also provides lower power consumption and larger scale integration than existing Gallium Arsenide and Indium Phosphide technologies.
The increasing demand for Internet and multimedia data is set to galvanize telecommunications carriers to deploy OC-768 transmission technologies that require vastly improved performance from ICs. According to Gartner Dataquest (Fiber Optic Food Chain, March 2001), the annual worldwide market for semiconductors used in fiber optic modules and physical layer ICs used for fiber optic communications is expected to reach US$11.7 billion in 2004.
MUX/DEMUX
Infineons multiplexer and demultiplexer are highly integrated circuits with 16 times 2.5 Gbit/s input channels multiplexed to a single serial 40 Gbit/s output data stream and vice-versa. The supported data-rates range from 39.8 Gbit/s up to 43 Gbit/s enabling out-of-band Forward Error Correction. The interfaces use Current Mode Logic, and both DC and AC coupling is supported. A 622 MHz and 2.5 GHz reference clock is provided and a Voltage Controlled Oscillator integrated onto each chip.
The multiplexer features Clock Management Unit functionality as well as a selectable 20 GHz and 40 GHz clock output to support both No Return to Zero and Return to Zero line coding, respectively. The demultiplexer integrates Clock and Data Recovery functionality with extremely high input sensitivity of 50mV. Both chips operate at a single 5.5V supply voltage.
Availability
The FOA4400 multiplexer chip and the FOA5400 demultiplexer chip as well as evaluation boards are now available.
About Infineon
Infineon Technologies AG, Munich, Germany, offers semiconductor and system solutions for applications in the wired and wireless communications markets, for security systems and smartcards, for the automotive and industrial sectors, as well as memory products. With a global presence, Infineon operates in the US from San Jose, CA, in the Asia-Pacific region from Singapore and in Japan from Tokyo. In the fiscal year 2000 (ending September), the company achieved sales of Euro 7.28 billion with about 29,000 employees worldwide. Infineon is listed on the DAX index of the Frankfurt Stock Exchange and on the New York Stock Exchange (ticker symbol: IFX). Further information is available at www.infineon.com
Information Number
INFCOM200106.080e
Press Photos
-
Infineon Introduces Industry's First OC-768 Silicon Germanium-based MUX/DEMUX Chipset at Supercomm to Take the Lead in the 40G SONET/SDH MarketPress Picture
JPG | 1.12 mb | 1535 x 1063 px