IBM, Infineon Develop Most Advanced MRAM Technology to Date - Develop highest density revolutionary memory technology

Jun 10, 2003 | Market News

Joint news release of Infineon Technologies and IBM



Kyoto, Japan (VLSI Symposia), June 10, 2003 - IBM and Infineon Technologies AG (FSE/NYSE: IFX) today announced they have developed the most advanced Magnetic Random Access Memory (MRAM) technology to date by integrating magnetic memory components into a high-performance logic base.

Today’s announcement could accelerate the commercialization of MRAM, a breakthrough memory technology with the potential to begin replacing some of today’s memory technologies as early as 2005. MRAM could lead to ‘instant on’ computers, allowing users to turn computers on and off as quickly as a light switch.

At the VLSI Symposia taking place here this week, IBM and Infineon are presenting their high-speed 128Kbit MRAM core. It is fabricated with a 0.18 micron logic-based process technology, the smallest size reported to date for MRAM technology. This small base enabled IBM and Infineon to incorporate the smallest MRAM memory-cell size of 1.4 square microns, which is about 20 million times smaller than the average pencil eraser top. By accurately patterning the magnetic structures within this small cell, IBM and Infineon researchers were able to control the memory reading and writing operations.

A memory technology that uses magnetic, rather than electronic, charges to store bits of data, MRAM could significantly improve portable computing products by storing more information, accessing it faster and using less battery power than the electronic memory used today. MRAM combines the best features of today's common memory technologies: the storage capacity and low-cost of Dynamic RAM (DRAM), the high speed of Static RAM (SRAM), and the non-volatility of flash memory. Since MRAM retains information when power is turned off, products like personal computers using it could start up instantly, without waiting for software to “boot up”.

IBM's MRAM work complements its pioneering and ongoing development of advanced embedded DRAM memory, which is commercially available today and offers advantages over traditional SRAM.

“MRAM has the potential to become the universal memory technology of the future,” said Dr T. C. Chen, VP Science and Technology, IBM Research. “This breakthrough demonstrates that MRAM technology is rapidly maturing and could fundamentally alter the entire memory marketplace within the next few years.”

“Nonvolatile memory technologies like MRAM will play a major role in technology lifestyle solutions and we want to be the number one semiconductor company in this area by having a product demonstrator jointly developed with IBM available early 2004. Together with Altis Semiconductor, a joint venture of IBM and Infineon, we will pave the way for production readiness of MRAM as early as 2005," said Dr. Wilhelm Beinvogl, CTO of the Memory Product Division, Infineon.

Detailed benefits of MRAM



The non-volatility attribute of MRAM carries significant implications, especially for mobile computing devices. Memory technologies like DRAM and SRAM require constant electrical power to retain stored data. When power is cut off, all data in memory is lost. A laptop computer, for example, works from a copy of its software stored in memory. When turned on, a working version of the software is copied from the hard-disk drive into memory, so the user can access it quickly. Every time the power is turned off and then back on, the process must start over. By using MRAM, the laptop could work more like other electronic devices such as a television or radio: turn the power on and the machine jumps almost instantly to life with settings just as you had left them.

Non-volatility can save power as well. Since MRAM will not need constant power to keep the data intact, it could consume much less than current random access memory technologies, extending the battery life of cell phones, handheld devices, laptops and other battery powered products.

The high-speed attribute of MRAM means that electronic products can more quickly access data, and MRAM’s high-density means greater storage capacity.

For downloadable MRAM images and an animation, visit: http://domino.research.ibm.com/comm/bios.nsf/pages/mramvlsi.html

IBM and Infineon MRAM developments



IBM Research pioneered the development of tiny, thin-film magnetic structures as early as 1974. In the late 1980s, IBM scientists made a string of key discoveries about the "giant magnetoresistive" effect in thin-film structures. These developments enabled IBM to create the first super-sensitive GMR read/write heads for hard-disk drives, stimulating dramatic increases in data density. Altering many of the GMR materials enabled IBM scientists to make the "magnetic tunnel junctions" that are at the heart of MRAM.

IBM and Infineon have more than 10 years experience with successful joint development of new chip technologies, including traditional Dynamic RAM (DRAM), logic and embedded-DRAM technologies. In November 2000, they established a joint MRAM development program. By combining IBM technology with Infineon's expertise in creating very high-density semiconductor memory, the companies believe MRAM products could be commercially available as early as 2005.

About IBM Research & Microelectronics Divisions



IBM Research is the world's largest information technology research organization, with more than 3,000 scientists and engineers at eight labs in six countries. IBM has produced more research breakthroughs than any other company in the IT industry. IBM's early work with MRAM has been conducted in cooperation with the U.S. Defense Advanced Research Agency (DARPA). For more information on IBM Research, visit http://www.research.ibm.com.

IBM Microelectronics is a key contributor to IBM's role as the world's premier information technology supplier. IBM Microelectronics develops, manufactures and markets state-of-the-art semiconductor, ASIC and interconnect technologies, products and services. Its superior integrated solutions can be found in many of the world's best-known electronic brands.

IBM is a recognized innovator in the chip industry, having been first with advances like more power-efficient copper wiring in place of aluminum, faster silicon-on-insulator (SOI) and silicon germanium transistors, and improved low-k dielectric insulation between chip wires. These and other innovations have contributed to IBM's standing as the number one U.S. patent holder for ten consecutive years. More information about IBM Microelectronics can be found at: http://www.ibm.com/chips.

About Infineon



Infineon Technologies AG, Munich, Germany, offers semiconductor and system solutions for the automotive and industrial sectors, for applications in the wired communications markets, secure mobile solutions as well as memory products. With a global presence, Infineon operates in the US from San Jose, CA, in the Asia-Pacific region from Singapore and in Japan from Tokyo. In fiscal year 2002 (ending September), the company achieved sales of Euro 5.21 billion with about 30,400 employees worldwide. Infineon is listed on the DAX index of the Frankfurt Stock Exchange and on the New York Stock Exchange (ticker symbol: IFX). Further information is available at http://www.infineon.com

Information Number

INFMP200306.089

Related Links