TTTech and Infineon to speed up the development in autonomous driving
Joint publication of TTTech and Infineon Technologies
Munich, Germany and Vienna, Austria – March 7, 2016 – Under the guidance of AUDI AG, TTTech developed the central platform control unit “zFAS” integrating various functionalities of advanced driver assistance systems (ADAS). The ECU also enables comprehensive fusion of sensor data. Microcontrollers from Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) safeguard that highest requirements towards computing performance and safety are met.
zFAS addresses the rapidly increasing performance demand of active and passive assistance systems. It enables new functions such as piloted driving on congested highways and piloted parking. Requirements concerning functional safety, connectivity and computing capacity have reached new levels. The demand is driven by functional integration and the fusion of safety critical sensor data. The developers of the multicore processing platform took this specifically into account: an important part of the platform controller is TTTech’s Deterministic Ethernet, a reliable, real-time-capable Ethernet backbone solution. It enables the combination of data traffic of different criticality with a high data throughput. Furthermore, TTTech’s TTIntegration is used as middleware to run the application functions on top of the networked multiple microcontrollers.
In alignment with Audi, TTTech selected AURIX™ TC297T microcontrollers from Infineon for zFAS. The AURIX family offers a broad range of microcontrollers including advanced multicore products for highest requirements. “We are delighted to provide our high-performance AURIX microcontrollers as the centerpiece for the future-proof platform solution zFAS,” said Thomas Boehm, responsible for Autonomous Driving MCUs at Infineon. “Thus, we are further expanding a fruitful partnership with TTTech.” Infineon’s AURIX TC297T microcontrollers with their lockstep architecture and a special safety management unit can host multiple safety-related functions up to ASIL D.
“zFAS marks a milestone for highly integrated platform control units for advanced driver assistance,” said Marc Lang, Director Sales & Marketing at TTTech Automotive. “Infineon’s advanced microcontrollers and TTTech’s real-time Ethernet solutions are key components for this innovative ADAS solution.”
In addition, based on Deterministic Ethernet and Infineon’s AURIX TC297T, TTTech has developed an evaluation platform for driver assistance system ECUs, called TTA Drive. It enables customers to quickly and simply integrate different application modules at an early stage of series development. This integration process is supported by a software named TTIntegration and a tool-set specifically developed for TTA Drive.
In the scope of a capital increase in March 2015, Infineon acquired a stake in TTTech which is specialized in highly reliable, networked and safety-relevant control systems in vehicles.
TTTech has been using Infineon solutions for years, including the powerful XC2287 CPU for the general purpose control unit family HY-TTC 50. Infineon’s AURIX microcontroller has further been integrated in TTTech’s new Automotive Ethernet switch Hermes for the evaluation of multiple communication standards including Audio-Video Bridging (AVB), Time-Sensitive Networking (TSN) and Time-Triggered Ethernet (SAE AS6802).
About TTTech Automotive GmbH
TTTech Automotive, a subsidiary of TTTech Computertechnik AG, brings networking scalability and flexibility to automotive customers. The company enables safe communication and networking – up to SIL3/ASIL D – for systems with different safety requirements according to IEC 61508 and ISO 26262. The modular, certified hardware and software solutions are used for serial production in the field of control and monitoring of electric and hybrid propulsion systems as well as for vehicle dynamics and driver assistance. To validate the vehicle functions, the product range is completed by intelligent data loggers and test equipment for networked systems.
More information about TTTech Automotive is available at www.tttech-automotive.com.
Press contact at TTTech Computertechnik AG
Marco Lehner, Marketing Communications
Phone: +43 1 585 34 34-473
Fax: +43 1 585 34 34-90
Email: pr@tttech.com
www.tttech.com
About Infineon
Infineon Technologies AG is a world leader in semiconductor solutions that make life easier, safer and greener. Microelectronics from Infineon is the key to a better future. In the 2015 fiscal year (ending September 30), the company reported sales of about Euro 5.8 billion with some 35,400 employees worldwide. Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the over-the-counter market OTCQX International Premier (ticker symbol: IFNNY).
Follow us: twitter.com/Infineon - facebook.com/Infineon - plus.google.com/+Infineon
Information Number
INFATV201603-038
Press Photos
-
Thomas Boehm, Director, Automotive Chassis & Safety Microcontrollers, Infineon Technologies AGBoehm_Thomas_Infineon
JPG | 810 kb | 1024 x 1535 px
-
Marc Lang, Direktor Sales & Marketing Automotive, TTTech Automotive GmbHLang_Marc_TTTech
JPG | 1.71 mb | 1469 x 2126 px