TRENCHSTOP™ Advanced Isolation package for discrete IGBTs

May 10, 2017 | Market News

Munich, Germany – 10 May 2017 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) introduces the new package technology TRENCHSTOP™ Advanced Isolation. It is available for TRENCHSTOP and TRENCHSTOP Highspeed 3 IGBTs for best-in-class thermal performance and simpler manufacturing. The two versions are performance optimized to replace both fully insulated packages (FullPAKs) as well as standard and high performance isolation foils. The new package targets applications like power factor correction (PFC) for air conditioner, uninterruptible power supply (UPS) and power converters for drives.

Conventional options for isolation, like FullPAKs or standard TO packages used with isolation material, are expensive and difficult to handle. Additionally, they are inadequate for the heat dissipation needs of the latest high power density IGBTs. TRENCHSTOP Advanced Isolation offers the same footprint as a standard TO-247, but with 100 percent isolation. However, there is no need for thermal isolation foils or thermal grease. Thanks to an effective and reliable thermal path from the IGBT die to the heatsink, the new package offers increased power density. It improves reliability, and reduces system and manufacturing costs.

By removing the need for isolation materials and thermal grease, designers can reduce assembly time by up to 35 percent. At the same time they improve reliability by eliminating misaligned foils. The thermal resistance (R th) of the new package is 50 percent lower than with a TO-247 FullPak and 35 percent lower than a standard TO-247 with an isolation foil. These improvements translate into a better performance such as a 10° C lower operation temperature than a FullPak with similar IGBT. Using the Advanced Isolation package, system efficiency can be increased by 0.2 percentage points over standard TO-247 with isolation foil.

The package also has a low coupling capacitance of just 38 pF, which means better EMI performance and potentially smaller filters. The improved thermal characteristics can also contribute to better reliability because the IGBT will run at a lower temperature which reduces stress on the component. Furthermore, the heatsink size can be reduced to help save system costs, due to these lower temperatures. Also due to lower cooling requirements, designers can alternatively choose to use the higher margin for increased power density.

Availability

TRENCHSTOP Advanced Isolation will be available during the 3 rd quarter of 2017, samples will be available in July. The initial product portfolio will feature IGBTs from 40 A to 90 A in 600 V. TRENCHSTOP Advanced Isolation will be showcased at PCIM 2017. More information is available at www.infineon.com\advanced-isolation.

Infineon at the PCIM 2017

At the PCIM 2017 tradeshow Infineon is presenting leading edge technology for efficient systems in industrial, consumer and automotive applications. Infineon’s demos for powering an energy-smart world are presented at booth #412 in hall 9 (Nuremberg, Germany, 16-18 May 2017). Information about the PCIM show highlights is available at www.infineon.com/pcim.

Information Number

INFIPC201705-051d

Press Photos

  • TRENCHSTOP Advanced Isolation features a thermal resistance (Rth) which is 50 percent lower than with a TO-247 FullPak and 35 percent lower than a standard TO-247 with an isolation foil. These improvements translate into a better performance such as a 10° C lower operation temperature than a FullPak with similar IGBT.
    TRENCHSTOP Advanced Isolation features a thermal resistance (Rth) which is 50 percent lower than with a TO-247 FullPak and 35 percent lower than a standard TO-247 with an isolation foil. These improvements translate into a better performance such as a 10° C lower operation temperature than a FullPak with similar IGBT.
    TRENCHSTOP_Advanced Isolation_HSIP247-3-1_Combi

    JPG | 57 kb | 990 x 768 px