All-in-one solution featuring the highest efficiency class: solar inverter from Fronius uses CoolSiC™ MOSFETs
Joint press release of Fronius International GmbH and Infineon Technologies AG
Munich, Germany, and Wels, Austria – 20 November 2020 – A few weeks ago Fronius International GmbH launched the Symo GEN24 Plus solar inverter. Its Multiflow technology makes it suitable for a wide range of applications supporting energy self-sufficiency. Not only does it provide power for direct use in the household, but it also offers an interface for energy storage systems. In addition, the hybrid inverter is designed for water heating and the charging of electric cars, and can be connected to external systems. All this thanks to silicon carbide (SiC) from Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) with an efficiency of over 98 percent. In combination with the high voltage storage from BYD, the Symo GEN24 Plus achieved a record value in the System Performance Index (SPI) of 94 percent in the 10 kW class. It was the only one in this combination to achieve Class A energy efficiency.
“SiC modules can be used to build very energy-efficient, robust, and reliable inverters,” said Andreas Luger, Head of R&D Power Electronics from the Solar Energy Business Unit at Fronius. “This technology enables a significant increase in switching frequency. Compared to the previous generation, the functionality is significantly improved, while its size remains comparable. Each device now also has an output for a secure power supply, and backup power, in addition to the standard connection options for a hybrid inverter.”
“To maximize the advantages of SiC, engineers from Fronius and Infineon have jointly optimized the layout and chip assembly of the modules,” said Peter Wawer, Division President Industrial Power Control at Infineon. “Ultimately, the close communication between the development teams enabled system advantages that correspond to customer needs. Based on our tried and tested Easy module, the inverter's booster stages now use 1200 V CoolSiC™ MOSFETs in combination with CoolSiC diodes. This full-SiC solution thus ensures maximum efficiency.”
Full-SiC is also used for the battery stage. One Easy 1B 1200 V with an R DS(on) of 45 mΩ is used in the bidirectional DC/DC converter. The inverter stage implements a SiC hybrid solution in an Easy 2B module, which has also been tailored to the needs of Fronius. The NPC1 topology combines silicon-based 650 V TRENCHSTOP™ 5 IGBTs and rapid diodes with CoolSiC Schottky diodes. The modules are controlled in all stages with an EiceDriver™ IC gate driver.
The combination of SiC MOSFET modules in the booster and battery input with hybrid modules in the inverter stage ensures the best possible ratio of efficiency and cost. As Infineon's SiC power semiconductors have a high power density, the Symo GEN24 Plus from Fronius offers many functions such as backup power, storage connection, multi-MPP tracker, and energy management. The inverter weighs only 24 kg and has a small volume (HWD 594 x 527 x 180 mm 3). Its active air-cooling can reduce the temperature of the power electronics parts, and thus extend service life. The inverter is available in the power classes 6, 8, and 10 kW. Fronius supplies this inverter primarily in Europe, South America, and Australia.
More information about Infineon's CoolSiC range is available at www.infineon.com/coolsic-mosfet. Further information on the Symo GEN24 Plus from Fronius is available here.
About Fronius Solar Energy
The Fronius Business Unit (BU) Solar Energy has been developing photovoltaic energy solutions and distributing its products through a global network of expert installation, service and sales partners since 1992. More than 24 Solar Energy subsidiaries, an export ratio of over 95 percent and a total output of more than 17 Gigawatts from installed inverters are testament to this. Its mission is to achieve 24 hours of sun. Day after day Fronius is hard at work turning this vision of a future in which 100% of the world’s energy needs are covered by renewable sources into a reality. With this in mind, Fronius develops energy solutions to generate, store, distribute and consume solar energy economically and intelligently.
About Fronius International GmbH
Fronius International is an Austrian company with headquarters in Pettenbach and other sites in Wels, Thalheim, Steinhaus and Sattledt. Founded by Günter Fronius in 1945, this long-standing company with a rich tradition will be celebrating its 75th anniversary in 2020. What began as a local one-man venture has grown into a global player with more than 5440 employees worldwide working in the areas of welding technology, photovoltaics and battery charging systems. Its export ratio of around 93 percent is achieved with 34 international Fronius subsidiaries and sales partners/representatives in more than 60 countries. Moreover, its innovative products and services and its portfolio of 1264 registered patents make it an innovation leader on the world market.
Enquiries:
Heidemarie Haslbauer
+43 664 88293709
Information Number
INFIPC202011-015
Press Photos
-
The Symo GEN24 Plus solar inverter from Fronius combines CoolSiC™ MOSFET modules in the booster and battery input with hybrid modules in the inverter stage. This ensures the best possible ratio of efficiency and cost.Fronius_Symo_GEN_24
JPG | 220 kb | 2126 x 1593 px
-
The Symo GEN24 Plus solar inverter from Fronius combines CoolSiC™ MOSFET modules in the booster and battery input with hybrid modules in the inverter stage. This ensures the best possible ratio of efficiency and cost.Fronius_Symo_GEN_24_transparent
JPG | 410 kb | 2126 x 1593 px