Infineon introduces Semper™ Secure – world’s most advanced, secured NOR Flash memory for automotive, industrial, and communications markets

Jun 16, 2020 | Market News

Munich, Germany, and San José, California – 16 June 2020 – With the acquisition of Cypress Semiconductor Corporation, Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) enhances its expertise in memory solutions. Infineon today announced the addition of Semper Secure to its award-winning Semper NOR Flash memory platform. Based on Semper NOR Flash’s field-proven and robust smart memory architecture, Semper Secure NOR Flash is the first memory solution to combine security and functional safety in a single NOR flash device to deliver the security, safety, and reliability required for the most advanced connected automotive, industrial, and communications systems.

The proliferation of connected systems is driving the need for ever greater system security. Semper Secure NOR Flash provides a trusted solution to meet demanding requirements and protects critical system information. Having a secured flash solution is especially important when the NOR Flash is placed outside of a processor, making it vulnerable to a variety of attacks. Semper Secure is the only NOR Flash solution that serves as a hardware root-of-trust to provide end-to-end protection. Additionally, the Semper Solution Development Kit enables easy system integration to accelerate time-to-market and reduce total cost-of-ownership.

“Having a secured connected system is a top priority for customers focused on protecting information and maintaining system integrity,” said Sam Geha, Head of Infineon Technologies LLC Memory Solutions. “As systems increasingly rely on external NOR Flash to protect code and data in connected systems, the need for added advanced cryptographic security in memory is growing. Our Semper Secure NOR Flash architecture adds to the already most functionally safe Semper products a secure subsystem to enable end-to-end persistent protection and efficiently protect a system from being compromised.”

“As flash moves outside of the host processor, it has grown increasingly important to find ways to secure embedded systems,” said Jim Handy, President of Objective Analysis. “Infineon's approach to secure the flash memory itself when it can no longer be embedded within the MCU is a compelling architecture that offers design engineers more versatility.”

The Semper Secure NOR Flash family includes AEC-Q100 automotive-qualified devices with an extended temperature range of -40 °C to +125 °C, supports 1.8-V and 3.0-V operating ranges, and is available in densities of 128 Mb, 256 Mb and 512 Mb. Semper Secure NOR Flash is designed and fully compliant to the ISO 26262 standard and is ASIL-B compliant and ready to be used in systems up to ASIL-D. The implemented EnduraFlex™ architecture simplifies system design by enabling optimization for high endurance or long data retention partitions. The devices are offered with Quad Serial Peripheral Interface (SPI), Octal SPI and HyperBus™ interfaces. The Octal and HyperBus interface devices are compliant with the JEDEC eXpanded SPI (xSPI) standard for high-speed x8 serial NOR Flash and offer a read bandwidth of up to 400 MBps.

Availability

Infineon’s 256 Mb Semper Secure NOR Flash devices are sampling to lead customers now, with volume production expected during the second quarter of 2021.

Further information is available at www.infineon.com/sempersecure

About Infineon

Infineon Technologies AG is a world leader in semiconductor solutions that make life easier, safer and greener. Microelectronics from Infineon is the key to a better future. In the 2019 fiscal year (ending 30 September), the Company reported sales of €8.0 billion with around 41,400 employees worldwide. With the acquisition of US-based Cypress Semiconductor Corporation in April 2020, Infineon has become a global top 10 semiconductor company.

Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the over-the-counter market OTCQX International Premier (ticker symbol: IFNNY).

Follow us: Twitter - Facebook - LinkedIn

Press Photos

  • Semper™ Secure is the first memory solution to combine security and functional safety in a single NOR flash device
    Semper™ Secure is the first memory solution to combine security and functional safety in a single NOR flash device
    Semper_Secure_English

    JPG | 380 kb | 3000 x 1688 px