A new Infineon protection diode, the smallest in the world, guards today’s portable electronic equipment against electrostatic discharge
Neubiberg, Germany – December 12, 2007 – On winter days, in the dry air of heated rooms, people often experience electrostatic discharges. Wearing a pullover or other item of clothing with synthetic fabrics can cause sparks fly – literally. The tiny flashes are discharges of static electricity that can be as powerful as 15,000 volts, with currents as high as 50 amperes. If the charge is grounded properly by earthed objects like radiators or water pipes, it does not do any harm. But if it discharges into a mobile phone or another consumer electronics device, it can seriously damage the highly integrated circuits inside – unless the device is protected by special ESD components known as TVS diodes.
Infineon, the technology leader in TVS diodes for electrostatic discharge protection, today unveiled the world’s smallest diode of this type. Just 0.6mm long, 0.3mm wide and 0.3mm high, it is smaller than a sugar crystal, yet it can safely dissipate charges as high as 20,000 volts and protect advanced electronic equipment like mobile phones, digital video and still cameras and MP3 players. With a response time of less than half a nanosecond, it also reacts to ESD discharges extremely fast. The new diode not only makes it possible to build smaller and more sophisticated electronic devices, it also helps to enhance their reliability and though quality.
Further information is available at www.infineon.com/esdprotection or at www.infineon.com/tvsdiodes.
A podcast is available at www.infineon.com/podcast.
About Infineon
Infineon Technologies AG, Neubiberg, Germany, offers semiconductor and system solutions addressing three central challenges to modern society: energy efficiency, communications, and security. In the 2007 fiscal year (ending September), the company reported sales of Euro 7.7 billion (including Qimonda sales of Euro 3.6 billion) with approximately 43,000 employees worldwide (including approximately 13,500 Qimonda employees). With a global presence, Infineon operates through its subsidiaries in the U.S. from Milpitas, CA, in the Asia-Pacific region from Singapore, and in Japan from Tokyo. Infineon is listed on the Frankfurt Stock Exchange and on the New York Stock Exchange (ticker symbol: IFX).
Information Number
INFAIM200712-026
Press Photos
-
The smallest transient voltage suppression (TVS) diodes in the world come from Infineon. With a footprint of just 0.6 x 0.3mm2 and a mere 0.3mm high, the diode is designed to protect the latest electronic communication and consumer devices against electrostatic overvoltages as high as 20kV.TVS_diode_ant
JPG | 428 kb | 944 x 731 px
-
The smallest transient voltage suppression (TVS) diodes in the world come from Infineon. With a footprint of just 0.6 x 0.3mm2 and a mere 0.3mm high, the diode is designed to protect the latest electronic communication and consumer devices against electrostatic overvoltages as high as 20kV.TVS_diode_finger
JPG | 996 kb | 1535 x 1151 px