HybridPACK™ Drive G2 Fusion: Infineon combines silicon and silicon carbide in a cutting-edge power module for e-mobility
Munich, Germany – 15 October 2024 – Affordability combined with high performance and efficiency is the key to making electric mobility accessible to a broader market. That's why Infineon Technologies AG is introducing the HybridPACK™ Drive G2 Fusion, establishing a new power module standard for traction inverters in the e-mobility sector. The HybridPACK Drive G2 Fusion is the first plug'n'play power module that implements a combination of Infineon’s silicon and silicon carbide (SiC) technologies. This cutting-edge solution provides an ideal balance between performance and cost efficiency, giving more choice in the optimization of inverters.
One of the main differences between silicon and SiC in power modules is that SiC has a higher thermal conductivity, breakdown voltage and switching speed, making it more efficient, but also more expensive than silicon-based power modules. With the new module, the SiC content per vehicle can be reduced, while maintaining vehicle performance and efficiency at a lower system cost. For example, system suppliers can realize nearly the system efficiency of a full SiC solution with only 30 percent SiC and 70 percent silicon area.
“Our new HybridPACK Drive G2 Fusion module underlines Infineon’s innovation leadership in the automotive semiconductor industry,” said Negar Soufi-Amlashi, Senior Vice President & General Manager High Voltage at Infineon's Automotive division. “Addressing the demand for greater e-mobility range, this technological breakthrough smartly combines silicon carbide and silicon. Integrated in a well-introduced module package footprint it offers compelling cost-performance ratio over pure silicon carbide modules without adding system complexity for automotive system suppliers and vehicle manufacturers.”
HybridPACK Drive G2 Fusion expands Infineon's HybridPACK Drive power module portfolio and can be quickly and easily integrated in vehicle components or modules without requiring complex adjustments or configurations. The HybridPACK Drive G2 Fusion module features up to 220 kW in the 750 V class. It ensures high reliability over the entire temperature range from -40 °C to +175 °C and improved thermal conductivity. The unique properties of Infineon's CoolSiC™ technology and its silicon IGBT EDT3 technology with very fast turn-on enable the use of a single gate driver or dual gate drivers. This allows easy re-design from full silicon or full SiC based inverters to a fusion inverter. Generally, Infineon's holistic expertise in SiC MOSFET and silicon IGBT technology, power module packaging, gate drivers as well as sensors enables premium products with cost savings at system level. One example is the integration of Swoboda or XENSIV™ Hall sensors in the HybridPACK Drive package for more precise and efficient motor control.
Infineon will showcase the new HybridPACK Drive G2 Fusion at electronica 2024 in Munich from November 12 to 15 (hall C3, booth 502).
Infineon at electronica 2024
At this year's electronica in Munich, Infineon presents innovative solutions for applications that address the challenges of our time. Semiconductors contribute in many ways to the green and digital transformation, helping to shape an all-electric society. At electronica 2024, Infineon offers the opportunity to explore sustainable technologies that are revolutionizing the mobility and automotive landscape, enabling sustainable buildings and smarter living, and promoting the growth of artificial intelligence with minimal ecological impact. The company will present intelligent and energy-efficient solutions for tomorrow's connected world from November 12 to 15 in Hall C3, Booth 502 under the motto “Driving Decarbonization and Digitalization. Together.” More information is available at www.infineon.com/electronica
About Infineon
Infineon Technologies AG is a global semiconductor leader in power systems and IoT. Infineon drives decarbonization and digitalization with its products and solutions. The company has around 58,600 employees worldwide and generated revenue of about €16.3 billion in the 2023 fiscal year (ending 30 September). Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the OTCQX International over-the-counter market (ticker symbol: IFNNY).
Information Number
INFATV202410-010
Press Photos
-
HybridPACK™ Drive G2 Fusion: Infineon combines silicon and silicon carbide in a cutting-edge power module for e-mobilityHybridPACKDrive_G2_Fusion
JPG | 181 kb | 2126 x 1160 px
-
Negar Soufi-Amlashi, Senior Vice President & General Manager High Voltage at Infineon's Automotive divisionNegar_Soufi-Amlashi
JPG | 246 kb | 640 x 820 px