What is an adapted salesname?
Because special characters (e.g. commas, dots or dashes) can be disturbing, the OPN will not contain any special characters. That means that the adapted salesname is not equal to the regular salesname. For microcontroller products the adapted salesname will never show the "SA" prefix and the temperature identifier (third digit in the salesname) is moved to the end of the adapted salesname. In very few cases salesnames also had to be adapted slightly in addition to the deletion of special characters due to a maximum length of the OPN of 24 digits.