Infineon introduces lower cost Bluetooth® long-range module, CYW20822-P4TAI040, for low power applications
Munich – 15 February 2024 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) today announced the CYW20822-P4TAI040, its latest Bluetooth® module that pushes the low-power and range boundaries for wireless connectivity in IoT and consumer electronics. This module is the most cost effective in its class, offers seamless integration, enhanced performance with Bluetooth low-energy long-range (LE-LR) support, and exceptional reliability for a wide range of applications. With the right combination of low power and high performance, Infineon’s CYW20822-P4TAI040 is designed to support the entire spectrum of Bluetooth LE-LR use cases including industrial IoT applications, smart home, asset tracking, beacons and sensors, and medical devices.
According to a recent report by ABI Research [1], future use cases will demand additional improvements across almost all metrics. These include industrial IoT applications such as sensing, robotics, beacons, smart home, and asset tracking. In response, Infineon's CYW20822-P4TAI040 Bluetooth module delivers unparalleled connectivity and performance, enabling customers to create innovative products in the IoT and consumer electronics space.
With extensive experience in delivering certified Bluetooth and Bluetooth LE modules, Infineon’s regulatory testing (FCC, ISED, MIC, CE) and certification process with the Bluetooth SIG is precise and rigorous. Its pre-certified modules are optimized for cost, size, power, and range.
“Infineon is thrilled to expand its Bluetooth portfolio with the introduction of the CYW20822-P4TAI040 Bluetooth module to help designers get to market faster,” said Anurag Chauhan, Director of Marketing for the Bluetooth product line at Infineon Technologies. “As a leader in the IoT area in delivering innovative new Bluetooth LE solutions, this new module is a testament to our customer commitment. This new module delivers low power, long range, and excellent RF performance to meet our customers evolving needs.”
Key features of the CYW20822-P4TAI040 Bluetooth module
- Superior Connectivity: The CYW20822-P4TAI040 module utilizes the latest Bluetooth 5.0 technology to support 1M, 2M & Coded PHY along with advertisement and data extension. This ensures seamless and stable wireless connectivity Bluetooth low-energy and long-range connections.
- Energy Efficiency: Infineon's advanced power management techniques in the CYW20822-P4TAI040 module enable optimized energy consumption, prolonging battery life in portable devices. As part of its decarbonization and digitalization efforts, the CYW20822-P4TAI040 module has a very low active power consumption of 1.3 mA (Rx @ -95 dBm) and 3 mA (Tx @ 0 dBm), along with a sleep current consumption of 2 μA with 32 KB RAM retention.
- Zero-Programming: The CYW20822-P4TAI040 module is pre-programmed via the EZ-Serial firmware to eliminate customer programming. This helps accelerate the time-to-deployment for Bluetooth-enabled IoT solutions.
- Compact Design: With its compact form factor of 10.5 x 20.2 x 2.3 mm³, the CYW20822-P4TAI040 module offers ease-of-integration into various IoT devices, wearables, and other space-constrained applications.
Availability
Infineon’s CYW20822-P4TAI040 Bluetooth LE module is currently sampling. More information is available at https://www.infineon.com/CYW20822-P4TAI040
About AIROC™ Wireless Connectivity Products
Infineon’s AIROC wireless products, including Wi-Fi®, Bluetooth, Bluetooth Low Energy and Wi-Fi and Bluetooth combos, have shipped more than a billion devices and are the go-to choice for IoT solutions. The broad portfolio includes high-performing, reliable, ultra-low-power products that deliver robust industry-leading performance.
[1] Source: ABI Research, The Continued Evolution Of Short-Range Wireless: New Technologies, Future Enhancements, And Emerging Market Opportunities
インフィニオンについて
Infineon Technologies AG is a global semiconductor leader in power systems and IoT. Infineon drives decarbonization and digitalization with its products and solutions. The company has around 58,600 employees worldwide and generated revenue of about €16.3 billion in the 2023 fiscal year (ending 30 September). Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the OTCQX International over-the-counter market (ticker symbol: IFNNY).
Information Number
INFCSS202402-063
Press Photos
-
Infineon’s CYW20822-P4TAI040 is designed to support the entire spectrum of Bluetooth LE-LR use casesCYW20822_Module
JPG | 826 kb | 2126 x 2004 px