1.5 billion chips sold: technology for passport and ID security on the rise

2018-6-21 | 市场新闻

London, United Kingdom, and Munich, Germany – 21 June 2018 – To date, Infineon Technologies AG (FSE: IFX/OTCQX: IFNNY) has sold 1.5 billion security chips with its awarded Integrity Guard technology. Infineon provides robust solutions for enabling the protection of today and tomorrow’s government-issued electronic ID documents like passports from potential security attacks. The technology features a complex digital security architecture. It includes a fully encrypted data path and a self-checking dual CPU core. Even if attackers eavesdrop on the data signals, all they see is encrypted and illegible information. Integrity Guard was developed for applications with high data security requirements for a particularly long life cycle.

“With Integrity Guard we provide an unrivalled security solution for the connected world through one of the world’s most advanced technologies,” said Thomas Rosteck, Division President of Chip Card & Security at Infineon Technologies. “At Infineon, we are proud that through Integrity Guard we have set the technological standard for chip-based security.”

Security technology inspired by the double helix of DNA

Integrity Guard is a security technology inspired by the storage and processing of information within living cells – more specifically, the double helix of DNA. The technical realization of this innovation equips controllers with robust digital mechanisms. These protect secure data and monitor security conditions. Through Integrity Guard, the controller reacts autonomously to security threats. At the core of this self-checking design is a double CPU that performs a continuous self-check of all operations. This results in “integrity protection” – hence the name “Integrity Guard.”

First time ever: Both CPUs use fully hardware-encrypted algorithms

Another key element of Integrity Guard is its comprehensive encryption of the entire data path, preventing plaintext from appearing in plain sight on chips. It is still the first time ever in the history of commercial security controllers that both CPUs make use of fully hardware-encrypted algorithms with different dynamic keys. This is only possible because Infineon, having facilitated the integration of real encrypted operations, has implemented the CPUs from scratch. Infineon’s SLE 78 family has set new standards for government ID projects. Building on this success, Infineon launched the SLC 52G as its next-generation security controller family. In combination with the existing SLE 78 product family, the extended SLC 52G portfolio is prepared to meet governmental identification requirements beyond 2020.

Awarded for outstanding innovation

Infineon’s Integrity Guard technology was awarded Germany’s Industry Innovation Award and Sesame Award – both honored the digital security technology for its outstanding innovation. The Federal Office for Information Security (BSI) confirmed the high level of security of Infineon’s Integrity Guard-based security chips, using the “Common Criteria” as a basis – the internationally recognized standard for the rigorous assessment and certification of security chips. More than 20 Common Criteria EAL 6+ Certificates, maintenance certificates or reassessments for security controllers based on Integrity Guard have been achieved. The security controller also meets the security requirements for payment cards from EMVCo*.

Infineon at the SDW 2018

At the SDW 2018 tradeshow Infineon is presenting state-of-the-art security technologies for future-proof eGovernment documents at booth J26 (London, United Kingdom, 25-27 June 2018). Thomas Pöppelmann will present latest findings in his speech on “Post-quantum cryptography: Challenges and opportunities for ID documents” on 27 June, 11.05 hours at Mountbatten, sixth floor.

Further details about the tradeshow are available at www.sdwexpo.com.

More information about security solutions from Infineon

Having delivered over 150 successful ID reference projects over the world, Infineon has been leading the security market for more than 30 years. In Europe alone, more than 75% of national eID projects already rely on Infineon solutions and 60% of smart healthcare cards worldwide do the same.

More information about Integrity Guard: www.infineon.com/integrityguard

More information about security solutions from Infineon: www.infineon.com/security


*Dual interface solutions support both contactless and contact-based technologies. The EMV® Chip Specifications define globally valid requirements for chip-based payment solutions and acceptance terminals. They enable secure contact and contactless applications and the use of other emerging payment technologies. Further information is available at www.emvco.com

Press Photos

  • Infineon has sold 1.5 billion security chips with its awarded Integrity Guard technology.
    Infineon has sold 1.5 billion security chips with its awarded Integrity Guard technology.
    IntegrityGuard

    JPG | 165 kb | 2126 x 2126 px

  • Infineon provides robust solutions for enabling the protection of today and tomorrow’s government-issued electronic ID documents like passports from potential security attacks.
    Infineon provides robust solutions for enabling the protection of today and tomorrow’s government-issued electronic ID documents like passports from potential security attacks.
    eGate

    JPG | 872 kb | 2126 x 1417 px

  • Even if attackers eavesdrop on the data signals, all they see is encrypted and illegible information. Integrity Guard was developed for applications with high data security requirements for a particularly long life cycle.
    Even if attackers eavesdrop on the data signals, all they see is encrypted and illegible information. Integrity Guard was developed for applications with high data security requirements for a particularly long life cycle.
    ID-Scan

    JPG | 737 kb | 2126 x 1417 px

  • “With Integrity Guard we provide an unrivalled security solution for the connected world through one of the world’s most advanced technologies,” said Thomas Rosteck, Division President of Chip Card & Security at Infineon Technologies. “At Infineon, we are proud that through Integrity Guard we have set the technological standard for chip-based security.”
    “With Integrity Guard we provide an unrivalled security solution for the connected world through one of the world’s most advanced technologies,” said Thomas Rosteck, Division President of Chip Card & Security at Infineon Technologies. “At Infineon, we are proud that through Integrity Guard we have set the technological standard for chip-based security.”
    ThomasRosteck

    JPG | 379 kb | 1134 x 1500 px