Infineon contributes to industry's highest power density grid storage ground power conditioner from Daihen with 2000 V SiC Module

2024-7-19 | 市场新闻

Munich, Germany, and Tokyo, Japan – 19 July 2024 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) announced that its CoolSiC™ 2000 V modules have been selected by Daihen Corporation for their innovative unit-type power conditioners for grid storage batteries. In the journey towards reducing carbon emissions, both grid storage batteries and the power conditioners that are linked to them play a vital role in facilitating the wider adoption of renewable energy sources like solar and wind power generation. There has been an increasing demand for higher voltage storage batteries and power conditioners to enhance the effectiveness of power generation, storage, and transmission. Moreover, with the expansion of storage battery systems on a larger scale, finding suitable locations and minimizing construction costs have emerged as significant challenges.

The unit-type power conditioner for grid storage batteries launched by Daihen in March 2024 is the first product in the industry to achieve connection to storage batteries at a high DC link voltage of 1500 V. The higher voltage enables the product to be used with large-capacity storage battery facilities, which has resulted in a 40 percent [1] reduction in the footprint of grid storage batteries compared to the conventional product.

The high power density is achieved by using Infineon's 62 mm CoolSiC MOSFET 2000 V module (FF3MR20KM1H). In addition to the characteristics of SiC that enable high voltage, better thermal dissipation and high power density, Infineon's SiC products feature M1H trench technology that increases the gate drive voltage range and provides high robustness and reliability against gate voltage spikes. Infineon was the pioneer in the industry to introduce the 2000 V class for a SiC module. This innovation has been instrumental in simplifying the inverter circuit configuration. Furthermore, the optimized 62 mm package has led to a substantial reduction in system size, contributing to enhanced efficiency and performance.

Mr. Akihiro Ohori, General Manager, Development Department, Energy Management System Division, Daihen, said, “In order to increase the voltage of power conditioners, the circuit configuration of conventional 1200 V devices had become complicated. However, by adopting Infineon's 2000 V SiC modules, we were able to achieve a simplified circuit configuration and control design, thereby reducing development resources and the footprint.”

Masanori Fujimori, Marketing Director of the Industrial & Infrastructure Segment at Infineon Technologies Japan, said, “We are very pleased that our pioneering CoolSiC 2000 V module has contributed to the development of the industry's highest power density power conditioners for grid storage batteries. We believe that Infineon's SiC technology will address the need for higher efficiency in energy storage systems and will greatly contribute to the growth of renewable energy.”

 

[1]   For grid storage batteries equivalent to 12MW/60M Wh. Comparison with Daihen's power conditioner for 1000 V storage batteries

 

About Infineon

Infineon Technologies AG is a global semiconductor leader in power systems and IoT. Infineon drives decarbonization and digitalization with its products and solutions. The company has around 58,600 employees worldwide and generated revenue of about €16.3 billion in the 2023 fiscal year (ending 30 September). Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the OTCQX International over-the-counter market (ticker symbol: IFNNY).

Further information is available at www.infineon.com

This press release is available online at www.infineon.com/press

Follow us: X - Facebook - LinkedIn

Information Number

INFGIP202407-026

Press Photos

  • The unit-type power conditioner for grid storage batteries by Daihen uses Infineon’s CoolSiC™ 2000 V modules.
    The unit-type power conditioner for grid storage batteries by Daihen uses Infineon’s CoolSiC™ 2000 V modules.
    Daihen_Power Conditioner_Unit

    JPG | 196 kb | 2126 x 1190 px