Successful Market Launch of Heat Conducting Paste TIM – Rapid Expansion of Range to other Product Groups

Apr 30, 2013 | Market News

Neubiberg, April 30, 2013 – The Thermal Interface Material (TIM) developed by Infineon Technologies AG for the reduction of contact resistance between the metal surface of power semiconductors and the heat sink has been launched successfully. Using the EconoPACK™ + of the new D Series, customers were able to see for themselves that conductivity was substantially improved with the heat conducting paste. As a result of strong customer demand, Infineon is now planning to expand the range. As early as in the last quarter of 2013 the module PrimePACKTM 3 and in the first quarter of 2014 the product groups 62mm, EconoDUALTM 3 and PrimePACKTM 2 are going to be available with TIM pre-applied. Toward the end of the first half of 2014 the modules EconoPACKTM 4 as well as the modules Econo 2 and 3 are to be available with the material. The launch of the TIM-applied production series Easy 1B and 2B, Smart 2 and 3, and IHM / IHV is planned for 2015.

In order to be able to meet the greatly increasing demand, Infineon has set up a production line for applying TIM to the modules at the Hungarian Backend site for power electronics in Cegléd. The thermally conductive paste is applied to the modules using a stencil-printing process. An elaborate quality assurance procedure integrated into the fabrication process guarantees that no air is trapped when joining the module and the heat sink. Special technical processes and machines were developed just for the fabrication process.

“TIM and the process developed by us for applying the paste makes it possible for the first time to assure a maximum value instead of typical values,” says Dr. Martin Schulz, the manager responsible for qualification in Application Engineering at Infineon Technologies AG. “Against the background of increasingly higher power densities, the thermal budget can now be planned more precisely in the design stage of applications.”

TIM allows significantly reduced contact resistance between the metal surface of the power semiconductor and the heat sink. The transfer resistance from module to heat sink for the new EconoPACK™ + D Series is reduced by 20 percent. This optimized thermal transfer improves the lifetime and reliability of modules. As the material functions reliably from the start, a special burn in cycle is not necessary as has been the case in the past for many comparable materials with phase-changing properties. The heat conducting paste is also free of silicone and electrically nonconductive.

More information

You’ll find more information about TIM and about the module types using it at www.infineon.com/TIM. Infineon will be presenting the power semiconductors with the heat conducting paste from May 14 to 16, 2013 at the PCIM trade show in Nuremberg in Hall 9, Booth 311. More information is available at www.infineon.com/PCIM2013.

About Infineon

Infineon Technologies AG, Neubiberg, Germany, offers semiconductor and system solutions addressing three central challenges to modern society: energy efficiency, mobility, and security. In the 2012 fiscal year (ending September 30), the Company reported sales of Euro 3.9 billion with close to 26,700 employees worldwide. Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the over-the-counter market OTCQX International Premier (ticker symbol: IFNNY).

Information Number

INFIPC201304.040

Press Photos

  • On Infineon's IGBT module EconoPACK™+ of the new D Series, the contact resistance between the module and heat sink drops by 20 percent with TIM. The optimized heat transfer extends both the service life and the reliability of the modules.
    On Infineon's IGBT module EconoPACK™+ of the new D Series, the contact resistance between the module and heat sink drops by 20 percent with TIM. The optimized heat transfer extends both the service life and the reliability of the modules.
    FS450R17OE5

    JPG | 508 kb | 1800 x 1200 px

  • On Infineon's IGBT module EconoPACK™+ of the new D Series, the contact resistance between the module and heat sink drops by 20 percent with TIM. The optimized heat transfer extends both the service life and the reliability of the modules.
    On Infineon's IGBT module EconoPACK™+ of the new D Series, the contact resistance between the module and heat sink drops by 20 percent with TIM. The optimized heat transfer extends both the service life and the reliability of the modules.
    FS450R17OE4

    JPG | 860 kb | 1800 x 1200 px