New diagnostic requirements in cars: Infineon is expanding its LED driver portfolio with the most flexible LED load diagnosis on the market
Munich, Germany, 8 November 2018 – LED lighting is taking over on the roads. It enables new design trends in cars, such as flexible styling and animation, and increases safety in traffic. If LEDs fail, this affects the reliability of the light. With LITIX™ Basic+, a new LED driver family , Infineon is launching the most flexible single LED short circuit diagnostic feature available on the market at electronica 2018. The new Active Retry function mode reduces the likelihood of misdiagnoses. This can save drivers unnecessary garage visits.
The American market and many German car manufacturers are now demanding LED drivers that are able to detect single LED short circuits. The LITIX Basic+ family includes three devices with this feature: TLD2132-1EP with one input and one output channel (1in/1out), TLD2131-3EP (1in/3out) and TLD2331-3EP (3in/3out). For fault diagnosis, they compare the voltage of the LED chain with a freely configurable reference voltage. The reference voltage can be adjusted by means of a resistor depending on the LEDs used and the expected working range.
In case of an error, the LED driver reports the status, e.g. to a microcontroller. Depending on the diagnostic requests from the system, it either deactivates the affected channel or leaves it activated. Unlike other solutions on the market, the LITIX Basic+ devices have the additional Active Retry option when the channel is deactivated. Active Retry describes the cyclic scanning of the LEDs by briefly reactivating the channels. This allows an automatic restart if the error condition no longer exists.
In addition to the single LED short circuit, LITIX Basic+ products detect both open load faults and short circuit to ground faults. Again, the diagnosis is flexibly configurable.
The LITIX Basic+ LED driver family consists of a total of six devices (single and three-channel versions) and supports an LED current range from 5 mA up to 360 mA. In addition to the devices with single LED short circuit detection, it offers two devices with an integrated PWM timer module (pulse width modulation): TLD2141-3EP (1in/3out) and TLD2142-1EP (1in/1out). This allows combined tail light functions (such as brake and tail light) to be implemented cost-effectively. The required light intensity is achieved precisely thanks to the pulse width modulation. With the TLD1114-1EP (1in/1out) device, the integrated power shift function allows power loss to be dissipated externally. Infineon LITIX Basic+ LED drivers complement the successful LITIX Basic family already on the market.
Availability
The products of the LITIX Basic+ family will be available to order from December. Further information is available at www.infineon.com/litix-basicplus.
Information Number
INFATV201811-012
Press Photos
-
The new Infineon LED driver family LITIX™ Basic+ provides the most flexible LED load diagnosis on the market.Litix_Basic
JPG | 302 kb | 1280 x 928 px