exceet Card expands banking business with SECORA™ Pay from Infineon

Apr 18, 2018 | Market News

Joint press release by exceet Card AG and Infineon Technologies AG

Munich, 18 April 2018 – exceet Card AG is further strengthening its portfolio with SECORA™ Pay security solutions from Infineon Technologies AG. Card manufacturers can easily integrate them thanks to the combination of dual interface chip technology with the award-winning Coil-on-Module (CoM) packages. These also make the card more robust and reliable.

“SECORA Pay provides us with certified EMV* solutions from a single source,” said Ulrich Reutner, CEO of exceet Card Group AG. “With Infineon’s support we were able to integrate the new technology very quickly into our product portfolio. We can thus meet rising demands concerning security and durability more easily, especially in the growing dual interface market.”

"Customers of Degussa Bank benefit from modern payment cards with dual interface technology," said Silke-Christina Kummer, Head of Card Business Advisory & Services at Degussa Bank AG. "We obtain Infineon SECORA Pay solutions from our card supplier exceet: Thanks to the coil-on-module packages, our customers not only receive a high-performance card, but also an extremely robust one.”

SECORA Pay: from contact-based to dual interface

Under the new brand SECORA™ Pay, Infineon combines outstanding hardware and software security solutions with the latest EMV applets to flexibly address regional market requirements. SECORA Pay supports a wide range of products and will thus significantly speed up migration from magnetic stripe to EMV-compliant payment cards with the focus on dual interface. 

“As the world’s leading provider of security controllers for payment cards, Infineon is teaming up with its partner to help the financial ecosystem taking advantage of state-of-the-art security solutions. Our flexible products offer outstanding performance independent from the used form factor,” said Bjoern Scharfen, Head of Payment & Wearables at Infineon. “SECORA Pay allows secure and efficient migration to the EMV standard.”

SECORA Pay S is a solution for payment cards that is quick to implement in the EMVCo environment and fully compliant with global standards and specifications. SECORA Pay X additionally supports domestic payment schemes and multi-application. It is also compatible with the CIPURSE™ open standard, enabling interoperable applications such as transport ticketing, access or closed loop payment.

About exceet Card AG

Exceet Card AG develops and manufactures advanced technologies and systems solutions in the areas of IT security, payment systems and Near Field Communication (NFC). This leading smart card provider offers data verification, personalization and mailing services. The core markets served are health, access, banking & financial transactions, corporate security and government.

Further information is available at: www.exceet-card-group.com

Contact at exceet Card AG

Fabian Rau

Phone: +49 89 33034-123

f.rau@exceet-card.com

 

 

 

*Dual interface solutions support both contactless and contact-based technologies. The EMV® Chip Specifications define globally valid requirements for chip-based payment solutions and acceptance terminals. They enable secure contact and contactless applications and the use of other emerging payment technologies.

Further information is available at: www.emvco.com

Information Number

INFCCS201804-048

Press Photos

  • Infineon SECORA Pay supports a wide range of products and will thus significantly speed up migration from magnetic stripe to EMV-compliant payment cards with the focus on dual interface.
    Infineon SECORA Pay supports a wide range of products and will thus significantly speed up migration from magnetic stripe to EMV-compliant payment cards with the focus on dual interface.
    Mobile-Payment

    PNG | 1.9 mb | 1500 x 1001 px

  • “As the world’s leading provider of security controllers for payment cards, Infineon is teaming up with its partner to help the financial ecosystem taking advantage of state-of-the-art security solutions. Our flexible products offer outstanding performance independent from the used form factor,” said Bjoern Scharfen, Head of Payment & Wearables at Infineon. “SECORA Pay allows secure and efficient migration to the EMV standard.”
    “As the world’s leading provider of security controllers for payment cards, Infineon is teaming up with its partner to help the financial ecosystem taking advantage of state-of-the-art security solutions. Our flexible products offer outstanding performance independent from the used form factor,” said Bjoern Scharfen, Head of Payment & Wearables at Infineon. “SECORA Pay allows secure and efficient migration to the EMV standard.”
    Bjoern-Scharfen

    JPG | 1.56 mb | 2126 x 1417 px

  • "Customers of Degussa Bank benefit from modern payment cards with dual interface technology," said Silke-Christina Kummer, Head of Card Business Advisory & Services at Degussa Bank AG. "We obtain Infineon SECORA Pay solutions from our card supplier exceet: Thanks to the coil-on-module packages, our customers not only receive a high-performance card, but also an extremely robust one.” – Source: Degussa 2018
    "Customers of Degussa Bank benefit from modern payment cards with dual interface technology," said Silke-Christina Kummer, Head of Card Business Advisory & Services at Degussa Bank AG. "We obtain Infineon SECORA Pay solutions from our card supplier exceet: Thanks to the coil-on-module packages, our customers not only receive a high-performance card, but also an extremely robust one.” – Source: Degussa 2018
    Degussa-1

    JPG | 177 kb | 1035 x 661 px

  • "Customers of Degussa Bank benefit from modern payment cards with dual interface technology," said Silke-Christina Kummer, Head of Card Business Advisory & Services at Degussa Bank AG. "We obtain Infineon SECORA Pay solutions from our card supplier exceet: Thanks to the coil-on-module packages, our customers not only receive a high-performance card, but also an extremely robust one.” – Source: Degussa 2018
    "Customers of Degussa Bank benefit from modern payment cards with dual interface technology," said Silke-Christina Kummer, Head of Card Business Advisory & Services at Degussa Bank AG. "We obtain Infineon SECORA Pay solutions from our card supplier exceet: Thanks to the coil-on-module packages, our customers not only receive a high-performance card, but also an extremely robust one.” – Source: Degussa 2018
    Degussa-2

    JPG | 152 kb | 1035 x 661 px