New sensing and balancing IC for battery management systems in electric cars

Jun 25, 2020 | Market News

Munich, Germany – 25 June, 2020 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) is expanding its product offering for battery management systems with a new sensing and balancing IC, the TLE9012AQU. The device is especially designed for batteries in hybrid and electric cars, but it is also suitable for other applications. It measures the voltage in up to twelve battery cells with an accuracy of ± 5.8 mV over the entire temperature and voltage range as well as the operating life cycle. Furthermore, it supports up to five external temperature sensors, provides an integrated cell balancing function and uses an iso-UART interface for communication.

Battery management systems (BMS) ensure, that the capacity of a battery is optimally utilized, i.e. that the longest possible range is achieved in an electric car, and that the battery does not age prematurely. In addition, they determine the battery's state of charge and state of health in order to estimate the available range and remaining service life. The TLE9012AQU provides the necessary measurement data and ensures a balanced state of charge through cell balancing. Among other things, this prevents the weakest cell from determining the total usable capacity of the battery.

To minimize the influence of interfering signals on the measurement results, the new sensing and balancing IC from Infineon features a programmable noise filter. In addition, it performs the measurement in all cells simultaneously so that the results remain comparable even in the presence of temporary interference factors. A compensation algorithm with integrated stress sensor and extended temperature compensation ensures the long-term stability of the measurements.

Cell balancing is achieved via twelve balancing switches integrated on the chip – one per channel. They are designed for currents up to 150 mA. For higher balancing currents, the device also supports external switches. In addition, the cell balancing can be programmed to stop without a signal from the microcontroller after a defined time of up to 32 hours or when the cell has reached a defined voltage. This allows the microcontroller to switch to sleep mode and thus save energy.

With its twelve channels, the TLE9012AQU is particularly suitable for batteries that are partitioned with twelve cells per module. One device is then required per module. The iso-UART interface for data exchange between these modules and with the microcontroller allows easy voltage isolation and ensures data integrity. The communication supports more than 20 serially connected devices and a ring topology. This ensures that even if a single device fails, the communication chain is not broken and the rest of the system remains functional.

Availability

In addition to the TLE9012AQU, Infineon is launching a matching iso-UART transceiver component (TLE9015QU). Both devices will be available in July 2020. Further information is available at   www.infineon.com/battery-management-ics.  

Virtual PCIM 2020 booth

This year, Infineon will run the PCIM 2020 completely virtually. As always, visitors can expect a comprehensive insight into product innovations and application solutions. With the broadest portfolio of power semiconductors – spanning silicon, silicon carbide (CoolSiC™) and gallium nitride (CoolGaN™) technologies – Infineon continues to set the benchmark. The online trade fair opens its doors starting 1 July 2020. Please click here to register.

Information Number

INFATV202006-075

Press Photos

  • TLE9012AQU is a new 12-channel BMS IC designed for battery systems in hybrid and electric vehicles
    TLE9012AQU is a new 12-channel BMS IC designed for battery systems in hybrid and electric vehicles
    Infineon-BMS-IC-TLE9012AQU

    JPG | 612 kb | 2126 x 1536 px

  • TLE9015QU is an iso-UART transceiver device matching Infineon’s new BMS-IC for hybrid and electric vehicles
    TLE9015QU is an iso-UART transceiver device matching Infineon’s new BMS-IC for hybrid and electric vehicles
    Infineon-Transceiver-TLE9015QU

    JPG | 595 kb | 2126 x 1536 px

  • Battery management systems in hybrid and electric vehicles ensure that the capacity of a battery is optimally utilized and that the battery does not age prematurely
    Battery management systems in hybrid and electric vehicles ensure that the capacity of a battery is optimally utilized and that the battery does not age prematurely
    Infineon-Battery-in-EV

    JPG | 521 kb | 2126 x 1536 px