Scaling up power: TRENCHSTOP™ IGBT7 Easy portfolio completed with additional current ratings

Apr 27, 2020 | Market News

Munich, Germany – 27 April 2020 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) adds new current ratings to its 1200 V TRENCHSTOP™ IGBT7 modules. This completes the Easy 1B and 2B portfolio, which is now offering power solutions for up to 11 kW in PIM and up to 22 kW in six-pack topologies with the latest chip technology. Customers have the choice: either to increase the power for the Easy 2B module by replacing the IGBT4 with IGBT7 technology, or to reduce the footprint for the same power by replacing the Easy 2B IGBT4 with the Easy 1B IGBT7 in specific cases. Like the previously launched TRENCHSTOP IGBT7 Easy modules, the new current ratings perfectly fit the design needs of industrial drives.

The TRENCHSTOP IGBT7 chip, compared to previous generations, provides higher power density, greatly reduced losses, and offers a high level of controllability for drives applications. All modules equipped with this new chip technology are designed to be backward pin compatible with the former generation TRENCHSTOP IGBT4 modules. This supports manufacurers in reducing the design cycle for any new inverter platform.

Based on the new micro-pattern trench technology, the TRENCHSTOP IGBT7 chips have a much lower static losses compared to the IGBT4 chips with the on-state voltage reduced by 20 percent. This brings significant loss reduction in the application, especially for industrial drives, which usually operate at moderate switching frequencies. The power modules feature a maximum allowed overload junction temperature of 175°C. Additionally, they have been designed for softer switching.

Availability

The complete 1200 V TRENCHSTOP IGBT7 EasyPIM™ and EasyPACK™ portfolio can be ordered now. Based on the customers’ needs, solder pin and TIM variants complement the offering. More information is available at www.infineon.com/IGBT7.

Information Number

INFIPC202004-051

Press Photos

  • Based on the new micro-pattern trench technology, the TRENCHSTOP™ IGBT7 chips of the Easy 1B/2B portfolio have a much lower static losses compared to the IGBT4 chips with the on-state voltage reduced by 20 percent. This brings significant loss reduction in the application, especially for industrial drives, which usually operate at moderate switching frequencies.
    Based on the new micro-pattern trench technology, the TRENCHSTOP™ IGBT7 chips of the Easy 1B/2B portfolio have a much lower static losses compared to the IGBT4 chips with the on-state voltage reduced by 20 percent. This brings significant loss reduction in the application, especially for industrial drives, which usually operate at moderate switching frequencies.
    TRENCHSTOP_IGBT7_Easy_1B

    JPG | 529 kb | 1712 x 1011 px

  • Based on the new micro-pattern trench technology, the TRENCHSTOP™ IGBT7 chips of the Easy 1B/2B portfolio have a much lower static losses compared to the IGBT4 chips with the on-state voltage reduced by 20 percent. This brings significant loss reduction in the application, especially for industrial drives, which usually operate at moderate switching frequencies.
    Based on the new micro-pattern trench technology, the TRENCHSTOP™ IGBT7 chips of the Easy 1B/2B portfolio have a much lower static losses compared to the IGBT4 chips with the on-state voltage reduced by 20 percent. This brings significant loss reduction in the application, especially for industrial drives, which usually operate at moderate switching frequencies.
    TRENCHSTOP_IGBT7_Easy_2B

    JPG | 688 kb | 1796 x 1206 px