Infineon partnering with Rompower: Expansion of the competence for system solutions of universal chargers
Munich, Germany – 09. January 2020 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) expands with Rompower its expertise for the development of universal chargers with high efficiency and compact design. These USB-PD chargers (Power Delivery) with the universal USB-C connector enable the power supply of e.g. monitors or smart speakers and charge the batteries of mobile devices such as smartphones or tablets. Today, these plugs already perform other functions, such as fast charging smartphones. Using the USB-PD technology, smartphones can be fully charged in less than an hour. USB-PD is made possible by the universal USB-C connector, which allows for higher data transfer and higher power transfer compared to widely established micro-USB and USB-A/B connectors.
The next development stage for all these functions will be permanently installed USB-PD wall outlets. With a maximum power output of 100 W made possible by the USB-PD standard, they not only support fast charging of mobile devices, but also function as permanently installed adapters. In the medium term, USB-PD charging sockets will be used in public buildings, such as airports and hotels, as well as in private households and will reduce the need for adapters and chargers.
Within the partnership, Infineon will contribute its semiconductor expertise, Rompower will offer its technologies and international know-how in the system area as well as in the construction of compact, small and highly efficient charging solutions. The first step is the development of system solutions for compact fast chargers for smartphones and USB-PD wall outlets.
About Rompower
Rompower Energy Systems Inc. was incorporated in 1994 in Tucson Arizona and is an internationally recognized research and development company in the field of power conversion. The primary goal of this engineering firm is to develop new technologies designed to meet the needs of the power conversion industry. Further information is available at www.rompower.com.
About Infineon
Infineon Technologies AG is a world leader in semiconductor solutions that make life easier, safer and greener. Microelectronics from Infineon is the key to a better future. In the 2019 fiscal year (ending 30 September), the Company reported sales of €8.0 billion with around 41,400 employees worldwide. Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the over-the-counter market OTCQX International Premier (ticker symbol: IFNNY).
Information Number
INFPMM202001-019