Infineon launches OPTIGA™ Authenticate IDoT solution for enhanced protection against counterfeit devices

Feb 25, 2021 | Market News

Munich, Germany – 25 February 2021 – Consumer devices, home appliances and industrial machines are constantly exposed to the risk of counterfeit spares and accessories. Fakes can compromise functionality, user safety and – as a result – brand value. To solve this problem, Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) launches the OPTIGA™ Authenticate IDoT anti-counterfeit turnkey solution which combines enhanced authentication with unprecedented levels of configuration flexibility. OPTIGA Authenticate IDoT is the industry’s leading embedded security solution that delivers enhanced hardware ECC-based security and outstanding flexibility to address customer and application requirements.

With an extended temperature range of -40° to +120 °C, the solution is ideal for industrial applications and supports the ever-growing and ubiquitous requirements for authentication. Use cases include single-use disposables for HVAC and water filters, rechargeable batteries for portable devices, light electric vehicles as well as computing and robotic systems in highly complex eMobility, industrial and IoT environments.

OPTIGA Authenticate IDoT is packaged in the proven and robust TSNP SMD housing measuring as little as 1.5 x 1.5 x 0.38 mm 3. It supports four ECC authentication modes: one-way, mutual, host binding and host support. Designers can select from three temperature ranges, two communication profiles, three sets of memory and four integrated secured decremental counters with secured lifecycle management, capless LDO and robust ESD protection. Furthermore, OPTIGA Authenticate IDoT provides unique on-chip turnkey digital certificates and key pairs.

Evaluation and development kits are provided to simplify the integration of the security solutions along with full SDK, host code library and C-base application programming interface (API) to offer a strong platform for easy application testing. These tools are based on the latest PSoC 6 BLE prototyping kit with full programmer and debugger, BLE and Wi-Fi capabilities.

Availability

OPTIGA Authenticate IDoT comes in a proven and robust package optimized for size-restricted devices and applications. Samples are available now. The security solutions will be on display at Infineon’s Embedded Solutions Conference. More information is available at www.infineon.com/OPTIGA-Authenticate-IDoT.

Infineon’s virtual Embedded Solutions Conference 2021

The acquisition of Cypress makes Infineon one of the world's top 10 semiconductor manufacturers. At the virtual Embedded Solutions Conference 2021 from 1 to 5 March 2021, visitors can see how the “new” Infineon makes the IoT work and explore the innovations and insights from the automotive, industrial, and IoT sectors. They can dive into Infineon’s market-leading portfolio, get into contact with the experts and catch up on the current trends by listening to more than 50 expert talks and product presentations. More information is available at www.infineon.com/embeddedworld.

Information Number

INFCSS202102-041

Press Photos

  • OPTIGA™ Authenticate IDoT protects OEMs and consumers against counterfeited devices. It is a turnkey solution which combines enhanced authentication with unprecedented levels of configuration flexibility.
    OPTIGA™ Authenticate IDoT protects OEMs and consumers against counterfeited devices. It is a turnkey solution which combines enhanced authentication with unprecedented levels of configuration flexibility.
    OPTIGA_Authenticate_IDoT_applications

    JPG | 672 kb | 2126 x 1503 px

  • OPTIGA™ Authenticate IDoT protects OEMs and consumers against counterfeited devices. It is a turnkey solution which combines enhanced authentication with unprecedented levels of configuration flexibility.
    OPTIGA™ Authenticate IDoT protects OEMs and consumers against counterfeited devices. It is a turnkey solution which combines enhanced authentication with unprecedented levels of configuration flexibility.
    OPTIGA_Authenticate_IDoT_water_filter

    JPG | 325 kb | 1503 x 2126 px