AIROC™ Wi-Fi & Bluetooth® combo chip brings reliable, high performance connectivity to TomTom's new satnav

Jun 21, 2021 | Market News

Munich, Germany, and Amsterdam, Netherlands – 21 June 2021 – TomTom GO Discover, developed by TomTom, the location technology company, is one of the quickest and most powerful satnavs on the market today. The satnav with its 5, 6, and 7-inch display leverages the AIROC™ CYW43455 Wi-Fi and Bluetooth® combo chip from Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY). The AIROC wireless solution combines Wi-Fi 5 (802.11 ac) and Bluetooth® 5.0 on a single chip and adds fast and robust wireless connectivity that is critical to the navigation device. Infineon’s AIROC family includes a broad range of wireless solutions that deliver reliable, high performance connectivity.

The TomTom GO Discover downloads map updates three times faster than other navigation devices, powered by the integrated 5 GHz Wi-Fi frequency band. Furthermore, with the integrated Bluetooth® interface, the TomTom GO Discover can also be connected to the smartphone, making both real-time traffic information and TomTom's premium live services available at all times. This includes up-to-date information on fuel prices, parking availability and the localization of charging points for electric vehicles.

“Built with safety in mind, the new TomTom GO Discover makes every journey more enjoyable,” said Mike Schoofs, Managing Director of TomTom Consumer. “With Infineon's AIROC wireless connectivity solutions, we have succeeded in fitting the satnav with powerful and fast wireless interfaces enabling the device's traffic and map information to be regularly updated. The chip allows us to combine our in-depth understanding of driver requirements with the latest and greatest technology.”

“The low power products from our AIROC wireless connectivity portfolio utilize advanced design and processing techniques to reduce power consumption during operation and sleep mode,” said Sivaram Trikutam, Senior Director IoT Compute and Wireless at Infineon. “In addition, the 1x1 chip integrates high-level hardware processes and algorithms that optimize the collaboration of WLAN and Bluetooth® for maximum performance. As a result, the chip is ideal for mobile navigation devices that require reliable wireless interfaces to provide drivers up-to-date information on traffic conditions and other relevant information.”

The AIROC wireless connectivity portfolio offers 1x1 Wi-Fi 5 (802.11ac), Bluetooth®, and operates in the 2.4 GHz and 5 GHz frequency spectrum. The Wi-Fi 5 mode supports 20 MHz, 40 MHz and 80 MHz channels for data rates up to 433.3 Mbps and all rates specified in 802.11a/b/g/n are also supported. This triples the throughput and transmission speed over WLAN and significantly improves scalability.

The high-data transmission speed proves particularly beneficial when streaming media such as HD videos, transferring and storing files, as well as for extending the range of Wi-Fi networks. Furthermore, the Wi-Fi 5 specification helps extend the battery life. Once the Wi-Fi interface has exchanged data at a high rate with its access point, the radio is immediately deactivated and goes back to sleep mode, reducing overall power consumption.

Availability

AIROC Wi-Fi & Bluetooth® combo chips are now available. More information is available at www.cypress.com/products/airoc-wi-fi-combos.

Information Number

INFCSS202106-078

Press Photos

  • The AIROC™ wireless solution for TomTom’s GO Discover satnav combines Wi-Fi 5 (802.11 ac) and Bluetooth® 5.0 on a single chip and adds fast and robust wireless connectivity that is critical to the navigation device. Infineon’s AIROC family includes a broad range of wireless solutions that deliver reliable, high performance connectivity.
    The AIROC™ wireless solution for TomTom’s GO Discover satnav combines Wi-Fi 5 (802.11 ac) and Bluetooth® 5.0 on a single chip and adds fast and robust wireless connectivity that is critical to the navigation device. Infineon’s AIROC family includes a broad range of wireless solutions that deliver reliable, high performance connectivity.
    AIROC_Wi-Fi_Bluetooth_Combo

    JPG | 484 kb | 1535 x 1447 px

  • The AIROC™ wireless solution for TomTom’s GO Discover satnav combines Wi-Fi 5 (802.11 ac) and Bluetooth® 5.0 on a single chip and adds fast and robust wireless connectivity that is critical to the navigation device. Infineon’s AIROC family includes a broad range of wireless solutions that deliver reliable, high performance connectivity.
    The AIROC™ wireless solution for TomTom’s GO Discover satnav combines Wi-Fi 5 (802.11 ac) and Bluetooth® 5.0 on a single chip and adds fast and robust wireless connectivity that is critical to the navigation device. Infineon’s AIROC family includes a broad range of wireless solutions that deliver reliable, high performance connectivity.
    GO-Discover_Front

    JPG | 262 kb | 1535 x 1008 px

  • The AIROC™ wireless solution for TomTom’s GO Discover satnav combines Wi-Fi 5 (802.11 ac) and Bluetooth® 5.0 on a single chip and adds fast and robust wireless connectivity that is critical to the navigation device. Infineon’s AIROC family includes a broad range of wireless solutions that deliver reliable, high performance connectivity.
    The AIROC™ wireless solution for TomTom’s GO Discover satnav combines Wi-Fi 5 (802.11 ac) and Bluetooth® 5.0 on a single chip and adds fast and robust wireless connectivity that is critical to the navigation device. Infineon’s AIROC family includes a broad range of wireless solutions that deliver reliable, high performance connectivity.
    GO-Discover_in_car_L_20Q4

    JPG | 256 kb | 1535 x 1024 px