Osram and Infineon jointly boost NFC programming for extended flexibility in LED luminaires configuration

Joint press release of Osram GmbH and Infineon Technologies AG

May 27, 2021 | Market News

Munich, Germany – 27 May 2021 – Reduced complexity together with increased functionality and efficiency are dominating the agenda of all lighting manufacturers. In this regard, Osram and Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) now join forces to enable Near Field Communication (NFC) programming for the industry. Osram’s new OPTOTRONIC ® FIT product family features Infineon’s NLM0011 and NLM0010 dual-mode NFC wireless configuration integrated circuits (ICs) with pulse width modulation (PWM). This will bring benefits at all levels of the LED luminaire value chain.

NFC programming is an emerging technology designed to replace the time-consuming resistor-setting techniques via a contactless NFC interface. The integrated constant lumen output (CLO) functions additionally help saving energy by maintaining the luminous flux constant over an extended luminaire lifecycle. The NFC interface solution allows for more cost-efficient, non-dimmable LED driver products.

Operational efficiency is improved by enabling automatic in-line or batch programming in production. It also creates significant flexibility throughout the entire LED value chain and LED luminaire life cycle: Luminaire parameters like lumen output and CLO settings can be programmed during the installation. The Osram Tuner4TRONIC Smartphone App supports fine-tuning and adaption to the desired lighting requirements.

“The combination of Osram’s market-leading LED Driver programming suite and Infineon’s ICs extend all the benefits of Near Field Communication to our entire awarded LED Driver range,” said Michael Huelskemper, Head of Product Management EMEA at Osram Digital Systems.

From LED driver and luminaire manufacturers to lighting service companies and end-user, advantages are numerous: reduced number of LED driver variants, simplified LED module selection, end-of-line configuration, and high output control precision. Besides, logistics efficiency is increased and costs for installation, cabling, and maintenance are reduced. The access to these features is fully controllable by the luminaire manufacturer thanks to security features provided by the App and the new IC.

“Infineon’s innovative NFC-PWM series enable the most cost-effective implementation of NFC programming. The integrated features such as the CLO function and the digital parameter setting help our customers to meet the contemporary LED design requirements. At the same time, they are also providing enhanced flexibility,” added Qi Zhu, Director Business Development Contactless Power and Sensing at Infineon’s Power & Sensor Systems Division.

More information about the NFC-PWM series is available at www.infineon.com/nfc-pwm.

 

ABOUT OSRAM

OSRAM, based in Munich, is a leading global high-tech company with a history dating back more than 110 years. Primarily focused on semiconductor-based technologies, our products are used in highly diverse applications ranging from virtual reality to autonomous driving and from smartphones to smart and connected lighting solutions in buildings and cities. OSRAM uses the endless possibilities of light to improve the quality of life for individuals and communities. OSRAM’s innovations enable people all over the world not only to see better, but also to communicate, travel, work and live better. OSRAM had approximately 21,000 employees worldwide as of end of fiscal 2020 (September 30) and generated revenue of around three billion euros from continuing activities. The company is listed on the stock exchanges in Frankfurt and Munich (ISIN: DE000LED4000; WKN: LED 400; trading symbol: OSR). Additional information can be found at www.osram.com.

Information Number

INFPSS202105-074

Press Photos

  • OSRAM’s OPTOTRONIC® FIT product family features Infineon’s NLM0011 and NLM0010 dual-mode NFC ICs. From LED driver and luminaire manufacturers to lighting service companies and end-user, advantages of NFC programming are numerous: reduced number of LED driver variants, simplified LED module selection, end-of-line configuration, and high output control precision.
    OSRAM’s OPTOTRONIC® FIT product family features Infineon’s NLM0011 and NLM0010 dual-mode NFC ICs. From LED driver and luminaire manufacturers to lighting service companies and end-user, advantages of NFC programming are numerous: reduced number of LED driver variants, simplified LED module selection, end-of-line configuration, and high output control precision.
    NLM0011_SOT-23_5pin

    JPG | 659 kb | 1770 x 1721 px

  • OSRAM’s OPTOTRONIC® FIT product family features Infineon’s NLM0011 and NLM0010 dual-mode NFC ICs. From LED driver and luminaire manufacturers to lighting service companies and end-user, advantages of NFC programming are numerous: reduced number of LED driver variants, simplified LED module selection, end-of-line configuration, and high output control precision.
    OSRAM’s OPTOTRONIC® FIT product family features Infineon’s NLM0011 and NLM0010 dual-mode NFC ICs. From LED driver and luminaire manufacturers to lighting service companies and end-user, advantages of NFC programming are numerous: reduced number of LED driver variants, simplified LED module selection, end-of-line configuration, and high output control precision.
    Osram_OT_FIT_NFC

    JPG | 212 kb | 2126 x 2126 px