Infineon expands Rust ecosystem for AURIX™ with HighTec’s ISO 26262 ASIL D qualified Rust compiler and other solutions

Apr 5, 2024 | Market News

Munich, Germany – 5 April 2024 – The Rust programming language with its unique memory safety features has emerged as a viable complement or potential substitute for C/C++ in automotive software development. Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY), together with partners like HighTec EDV-Systeme now further expands the Rust ecosystem for its AURIX™ microcontrollers. HighTec just released the first ISO 26262 ASIL D qualified Rust compiler for AURIX TC3x and TC4x which ensures the software’s reliability and performance necessary to meet the rigorous requirements of the automotive industry. The overall Rust ecosystem for AURIX also includes Infineon’s peripheral access crates (PAC) for the TC37x, a set of Bluewind peripheral drivers, the Rust runtime NOS from Veecle as well as tools from Lauterbach and PLS which allow customers to evaluate and develop safe and secure applications with Rust.

HighTec’s ISO 26262 ASIL D qualified Rust compiler comes with a preconfigured cargo build system for seamless access to the Rust ecosystem for AURIX, including I/O crates, drivers, a Rust runtime, example projects including use cases with a mixed integration of Rust with C/C++, and a Rust integration of PXROS-HR, HighTec's safety-certified real-time operating system. HighTec’s compiler complements its proven C/C++ compiler for AURIX, which is also based on the cutting-edge open source LLVM compiler technology. Together they ensure a seamless integration of Rust code with legacy C/C++ code for the best possible interoperability between both languages.

“This hybrid approach is probably the most interesting, as many projects using Rust are expected to re-use legacy code and to preserve the C/C++ investment,” said Mario Cupelli, CTO at HighTec. “We are proud to contribute to Infineon’s Rust ecosystem with the first safety-qualified Rust compiler, supporting AURIX customers in developing secure, safer and more efficient applications.”

“Rust enables developers to leverage the benefits of our MCUs to minimize safety risks, shorten development cycles, and reduce costs. In the automotive industry, integration of a robust software ecosystem is crucial as tools are required to meet automotive-grade standards”, said Thomas Schneid, Senior Director Software, Partnership and Ecosystem Management at Infineon. “We are looking forward to collaborate with our Rust partners like HighTec to provide a complete Rust ecosystem for AURIX.”

The Rust ecosystem for AURIX furthermore includes Infineon’s newly released PAC for TC37x as starting point for TC3x and TC4x. Together with a set of Bluewind peripheral drivers written in Rust using the PAC, customers can evaluate the benefits of the hardware access via Rust. The included Rust runtime NOS from Veecle integrates AURIX with PXROS-HR; Lauterbach and PLS have added improved Rust support for their AURIX solutions. The new extended AURIX Rust ecosystem also includes a full set of documentation.

Availability

Registration to access the Rust ecosystem for AURIX is available at hightec-rt.com/rust-evaluation or www.bluewind.it/rust/ or veecle.io/aurix. At embedded world, visitors can see demos of the Rust ecosystem for AURIX at the booths of HighTec (hall 4, stand 4-432) and Bluewind (hall 5, stand 5-277). Further information on the Rust ecosystem for AURIX is available at https://www.infineon.com/cms/en/product/promopages/rust/

Infineon at Embedded World

Embedded World will take place in Nuremberg, Germany from 9 to 11 April, 2024. Infineon will present its products and solutions for decarbonization and digitalization in hall 4A, booth #138 and virtually. Company representatives will also hold several TechTalks as well as presentations at the accompanying Embedded World Conference, followed by discussions with the speakers. If you are interested in interviewing an expert at the show, please email media.relations@infineon.com . Industry analysts interested in a briefing can email MarketResearch.Relations@infineon.com . Information about the Embedded World show highlights is available at www.infineon.com/embeddedworld

About Infineon

Infineon Technologies AG is a global semiconductor leader in power systems and IoT. Infineon drives decarbonization and digitalization with its products and solutions. The company has around 58,600 employees worldwide and generated revenue of about €16.3 billion in the 2023 fiscal year (ending 30 September). Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the OTCQX International over-the-counter market (ticker symbol: IFNNY).

Follow us: X - Facebook - LinkedIn

Information Number

INFATV202404-089

Press Photos

  • Infineon Technologies, in collaboration with partners like HighTec EDV-Systeme, is expanding the Rust ecosystem for its AURIX™ microcontrollers, including an ISO 26262 ASIL D qualified Rust compiler.
    Infineon Technologies, in collaboration with partners like HighTec EDV-Systeme, is expanding the Rust ecosystem for its AURIX™ microcontrollers, including an ISO 26262 ASIL D qualified Rust compiler.
    Infineon_AURIX_TC4x

    JPG | 191 kb | 2126 x 1752 px