Infineon introduces the OPTIGA™ Trust M MTR, making it easy to add Matter and security to smart home devices
Recording of Online Media Briefing
Munich, Germany – 21 February, 2024 – In a world of increasing connectivity and the growing popularity of the Internet of Things, it is important to simplify interoperability across connected devices and to enhance their security and reliability. The Matter standard 1 was created precisely for this purpose. In order to facilitate integration of the Matter standard and security features into smart home and smart building devices, Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) now introduces the OPTIGA™ Trust M MTR. The Matter-certified Secure Element is the latest configuration of Infineon’s OPTIGA Trust M, combined with a Matter provisioning service.
Matter: smooth interoperability of connected devices
According to ABI Research forecasts, the number of smart home devices will double by 2030, reaching about 1.7 billion worldwide. All these devices have to be able to connect securely and reliably with each other and with different smart home ecosystems. That’s where the Matter standard comes into play, facilitating smooth interoperability across connected devices even from different companies. The Matter protocol defines a set of principles that support uniform security and privacy measures for the smart home, since smart homes rely on smart devices to increase not only comfort but also efficiency and security.
“When we designed the Matter protocol in the Connectivity Standards Alliance, we were committed to building in strong security,” said Steve Hanna, Distinguished Engineer at Infineon and leader of the standards teams that defined Matter’s security. “That’s why Matter brings new security features to the smart home, some of which were challenging for IoT product designers. Infineon’s OPTIGA Trust M MTR addresses those challenges head-on so that now it can be even easier to build a Matter product.”
OPTIGA Trust M MTR facilitates Matter and security integration
The tamper-resistant security controller can be easily integrated into a system to perform security-related functions and provide a high level of protection for sensitive data and cryptographic operations. As a discrete Secure Element, OPTIGA Trust M MTR can be integrated into any MCU-based design to enhance security and handle multiple product protocols simultaneously. This gives original equipment manufacturers greater flexibility and allows faster time to market.
According to the Matter protocol, every smart home device must have a Device Attestation Certificate (DAC), containing the Product ID (PID) and the Vendor ID (VID), to verify the authenticity and trustworthiness of each device commissioned in the Matter ecosystem. With OPTIGA Trust M MTR, the PID no longer needs to be defined in advance when the reel is ordered or manufactured. Instead, each device receives a personalized DAC injection at a later point right up until the start of device production. This gives device manufacturers more flexibility in creating multiple product variants of smart home devices.
OPTIGA Trust M MTR Secure Elements are pre-provisioned at a Common Criteria-certified Infineon facility. The batch of Secure Elements on a reel is shipped with an associated barcode. The customer claims ownership of these chips on the IoT portal of Infineon partner Kudelski IoT by scanning the barcode. Kudelski IoT is a trusted and established Product Attestation Authority (PAA) approved by the Connectivity Standards Alliance (CSA). Kudelski IoT will enable the download of production DACs corresponding to the vendor and the product. Finally, the personalized DAC is transferred to the OPTIGA Trust M MTR at the factory level (see graphic).
Availability
Samples of OPTIGA Trust M MTR are available now together with the OPTIGA Trust M MTR Shield for easy evaluation and design-in. Availability for the broad market will begin in March 2024. In addition, developers can rely on design-in application notes and extensive host-side integration support without having to sign a non-disclosure agreement (NDA). Moreover, Infineon offers training measures for the security products. More information is available at www.infineon.com/OPTIGA-Trust-M-MTR.
Please note: An Online Media Briefing will be held on 22 February, 2024 (3:00 pm CET / 9:00 am EST), in which Distinguished Engineer Steve Hanna will present additional information about the new OPTIGA Trust M MTR.
1 About Matter: In order to enhance the security and reliability of smart devices, Infineon and more than 600 companies are collaborating in the Connectivity Standards Alliance (CSA) to simplify and harmonize the Internet of Things using technology standards such as Matter. Matter was created to keep devices and information protected and private, yet easy to use. The Matter standard provides guidance to device manufacturers, enabling them to select the appropriate platform security for their devices and corresponding use cases. Matter embeds privacy principles into all interactions between devices and software agents that handle personal data. Ultimately, it creates the foundation for connected things by supporting simplicity, interoperability, reliability and security.
About Infineon
Infineon Technologies AG is a global semiconductor leader in power systems and IoT. Infineon drives decarbonization and digitalization with its products and solutions. The company has around 58,600 employees worldwide and generated revenue of about €16.3 billion in the 2023 fiscal year (ending 30 September). Infineon is listed on the Frankfurt Stock Exchange (ticker symbol: IFX) and in the USA on the OTCQX International over-the-counter market (ticker symbol: IFNNY).
Further information is available at www.infineon.com
This press release is available online at www.infineon.com/press
Information Number
INFCSS202402-065
Press Photos
-
OPTIGA Trust M MTR: the easiest way to add secured Matter compatibility to an existing design.INFIN_OPTIGA-Trust-M-MTR
JPG | 417 kb | 2126 x 1181 px
-
The new process of building Matter devices with OPTIGA™ Trust M MTR – simple, easy and secured.INFIN_OPTIGA-Trust-M-MTR_Graphic_Process
JPG | 142 kb | 1200 x 600 px