Infineon, Xilinx and Xylon team up for new microcontroller solutions in safety-critical applications

2019-2-22 | 市场新闻

Munich, Germany – 22 February 2019 – In order to provide more flexibility in how to use safety microcontrollers in automotive and industrial applications, Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) cooperates with Xilinx Inc. and Xylon, d.o.o.. At the Embedded World trade fair 2019, they present a new Xylon IP core called logiHSSL. It enables high-speed communication between Infineon’s AURIX™ TC2xx and TC3xx microcontrollers and Xilinx’ SoC, MPSoC and FPGA devices via the Infineon High Speed Serial Link (HSSL). This serial link supports baudrates of up to 320 Mbaud at a net payload data-rate of up to 84%.  

The HSSL is an Infineon native interface, low-cost in regards to pin-count as it requires only five pins – two LVDS with two pins each and one clk pin. So far, the HSSL interface is used to exchange data between AURIX devices and customer ASICs for performance or functional extension. Now, the new IP core will allow system developers to combine safety and security provided by AURIX with the wide range of functional possibilities brought to the table by the Xilinx devices. Linked devices can access and control each other’s internal and connected resources through the HSSL.

“Our AURIX microcontrollers are the market reference for many safety-critical applications, for example in advanced driver assistance and automated driving,” said Ralf Koedel, Marketing Director Microcontrollers at Infineon. “Now, we are creating new options for our customers in emerging applications that are both performance-hungry and safety-critical. Besides the ones mentioned these include for example industrial automation applications.”

“Our products are adopted in ADAS and AD architectures for data aggregation, pre-processing, and distribution as well as compute acceleration,” said Paul Zoratti, director Automotive Solutions, Xilinx. “Coupled with the AURIX family providing ASIL D level functional safety, this has created a strong market pull for an FPGA-based HSSL solution. Xylon’s licensable IP core will enable customers to implement a reliable HSSL communications path between Xilinx and Infineon devices without expending valuable development resources.”

To support development activities the partners are offering a starter kit. It includes a Xilinx evaluation kit, an Infineon AURIX evaluation board and a Xylon FMC board. Kit deliverables include the reference design with the test software application, Xylon’s logicBRICKS evaluation licenses, documentation and technical support.

At the Embedded World trade fair 2019 Infineon (booth #231, hall 3A) and its distribution partner EBV (booth #229, hall 3A) will show demo boards.

Availability

The new IP core and the development kit will be available starting in March 2019. Further information is available here.

Infineon at Embedded World 2019

Visit Infineon at Embedded World 2019 Exhibition & Conference (Nuremberg, Germany; 26-28 February 2019) at booth 231 in hall 3A. Highlights include solutions for smart, safe vehicles that drive automated; connected, secure factories; smart homes and consumer devices; as well as highly efficient and sophisticated drones. More information is available at www.infineon.com/embeddedworld.

Press Photos

  • A new IP core will enable high-speed communication between Infineon’s AURIX™ microcontrollers and Xilinx’ devices via HSSL.
    A new IP core will enable high-speed communication between Infineon’s AURIX™ microcontrollers and Xilinx’ devices via HSSL.
    AURIX_Safety_meets_Performance

    JPG | 1.52 mb | 5400 x 3900 px