New Infineon System Basis Chips are the first to allow high speed communication with up to 5 Mbit/s
Munich, Germany – 3 September 2018 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) is launching two new System Basis Chip (SBC) families: Lite and Mid-Range+. They are the first SBCs on the market supporting the ISO CAN FD protocol for communication at 5 Mbit/s for a large variety of automotive applications.
An SBC is the central supply of power and communication for microcontrollers within electronic control units (ECU) in cars. SBCs are integrated circuits (IC) that combine voltage supplies, communication bus interfaces (CAN, LIN) and supervision features. The combination of these three elements in one chip leads to lower system costs and up to 80 percent smaller design footprint compared to discrete solutions.
The new Infineon Lite SBCs are the entry level SBCs at optimized system costs. They incorporate one CAN transceiver to address a broad range of applications such as in-cabin wireless charger, NO x sensor, gear shifter or light control units. The Mid-Range+ SBCs are more powerful devices with one CAN and up to two LIN transceivers to support e.g. body control modules and gateway modules.
Recent developments in the automotive industry require increasingly faster communication capabilities. Originally, the CAN FD protocol was established for software updates during production and service events. Today, also the communication within the car and its connectivity to the outside world require an increased bandwidth and longer payload. For example, high-end front light applications such as matrix LED lighting require a large amount of data provided by camera systems and sensors to ensure a glare-free high beam.
In addition to high-speed communication, the new Infineon SBCs allow a lower power consumption. With their optional partial networking feature they reduce current consumption by putting the ECU in a sleep or stop mode when it is not needed. The Lite SBC family also features a charge pump to drive high side n-channel power MOSFETs. It can disconnect an external load during sleep mode in order to further reduce quiescent current.
All devices of the new SBC families include diagnostic and supervision features to support ECU functional safety concepts like under-voltage monitoring, window watchdog with reset, fail-safe operating mode and fail-safe output. Moreover, with the Mid-Range+ family external loads can be driven by four high-side switches.
The new Infineon SBCs offer high flexibility to designers. They are scalable regarding the number of communication interfaces and are software compatible with other Infineon SBC families such as the DCDC and Multi-CAN Power SBC families (TLE94x1, TLE926x & TLE927x).
Availability
The Mid-Range+ family is now available in the market, the Lite SBC family will be in October 2018. More information is available at www.infineon.com/SBC.
Information Number
INFATV201808.079
Press Photos
-
Mid-Range+ System Basis Chips allow communication with up to 5 Mbit/s and incorporate one CAN and up to two LIN transceiversMid-Range-SBC-TLE9263-3BQX
JPG | 172 kb | 1500 x 897 px
-
Lite System Basis Chips allow communications at 5Mbit/s and are designed for optimized system costs.Lite-SBC-TLE9461-3ES
JPG | 301 kb | 1500 x 975 px
-
Lite System Basis Chips allow communications at 5Mbit/s and are designed for optimized system costs.Lite-SBC-TLE9471-3ES
JPG | 301 kb | 1500 x 975 px