Electrifying cars: Infineon ready for strong growth in mild hybrid vehicles
Munich, Germany – 12 March 2020 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) expects significant growth in automotive 48 V systems in the coming years and is expanding its portfolio of suitable power devices. The chip manufacturer is launching new packages for its 80 V and 100 V MOSFETs with OptiMOS™ 5 technology to meet the different requirements of different 48 V applications. In view of the expected increase in demand, Infineon has set up a new manufacturing process to now produce the chips on its line for 300-millimeter thin-wafers in Dresden, Germany.
"In this decade, we will reach the point where the majority of all newly produced cars worldwide have a partially or fully electric powertrain," said Stephan Zizala, Vice President and General Manager Automotive High Power at Infineon. "According to market research, production of models with 48 V power supply and a mild hybrid drive is likely to increase more than tenfold between 2020 and 2030. In addition to our portfolio for high-voltage systems in battery-electric drives as well as full and plug-in hybrids, we therefore also strengthen our offering for 48 V systems with new devices and expanded supply capacities.”
Portfolio expansion at both ends of the power spectrum
Infineon offers a variety of 80 V and 100 V MOSFETs in OptiMOS 5 technology with very low, scalable on-state resistances down to 1.2 mΩ. For the core applications of a mild hybrid, for example starter generators, battery switches and DC-DC converters, where high power densities are required, Infineon is expanding its TOLx package family. This is based on the established TOLL (TO-Leadless, 10 mm x 12 mm) product for standard copper substrate PCBs and currents up to 300 A.
In addition, the family comprises the TOLG (TO Leads Gullwing Design) package with identical footprint for Insulated Metal Substrates (IMS) with aluminum core. Since the thermal expansion coefficients of copper and aluminium differ, the use of IMS boards under high thermo-mechanical stress leads to increased stress on the soldered connections between package and PCB. In order to mitigate this stress, the TOLG package is equipped with gullwing leads.
New package for top-side cooling
In the next step, Infineon will expand the TOLx family with a third member that is unique among the competition: the TOLT (TO Leads Top-Side Cooling) package. It enables heat dissipation through top-side cooling via the top of the package instead of via the PCB. This allows an increase in power of more than 20 percent and reduces the necessary cooling effort on the board. The start of volume production of TOLT products is planned for 2021.
Next to the TOLx family, Infineon also expands the package portfolio addressing less power-hungry auxiliaries such as fans and pumps that are also increasingly being transferred to the 48 V supply. Completely new are versions in the small S3O8 package (3.3 mm x 3.3 mm) for lower currents up to 40 A. They complement products with the slightly larger SSO8 package (5 mm x 6 mm) for currents up to 100 A that were added to the portfolio recently.
Mild hybrid drives based on a 48 V supply are a fast and cost-effective way for car manufacturers to achieve lower CO 2 fleet emissions . Among other things, they allow a higher recuperation energy compared to a 12 V system and use the energy gained for electrical support of the combustion engine. In addition, a 48 V supply offers performance and efficiency advantages for safety and comfort functions with high current loads, such as stability control or air-conditioning compressors. Depending on the configuration of the drive system and the number of auxiliary units, a mild hybrid can reduce CO 2 emissions by up to 15 percent compared to a pure combustion engine.
Availability
Products in TOLL, TOLG, SSO8 and S3O8 packages are now available. The start of volume production of TOLT products is planned for early 2021. Further information is available at www.infineon.com/automotivemosfet.
Information Number
INFATV202003-040
Press Photos
-
The TOLT package enables top-side cooling, which allows a power increase of more than 20 percent and reduces the necessary cooling effort on the board.OptiMOS-5_TOLT_Package
JPG | 581 kb | 2126 x 1317 px
-
The TOLG package complements the TOLx package family. It is designed for the use with IMS boards.OptiMOS-5_80V-100V_TOLG_Package
JPG | 568 kb | 2126 x 1176 px
-
The SSO8 package for currents up to 100 A is designed for 48 V auxiliaries such as pumps and fans.OptiMOS_80V-100V_SSO8_Package
JPG | 601 kb | 2126 x 1182 px
-
The S3O8 package is suitable for currents up to 40 A in less power-hungry 48 V auxiliaries.OptiMOS-5_80V-100V_S3O8_Package
JPG | 419 kb | 2126 x 1118 px