Flexibility meets increased power density and performance: Infineon enhances 1200 V EconoDUAL™ 3 portfolio with IGBT7 featuring new current ratings
Munich, Germany – 6 September 2021 – Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) launches new current ratings for its EconoDUAL™ 3 portfolio with TRENCHSTOP™ IGBT7 chips. With the broad range of current classes from 300 A up to 900 A, the portfolio offers inverter designers a high degree of flexibility while also providing increased power density and performance. In addition to solar and drive applications, the portfolio is also tailored for commercial, construction and agricultural vehicles (CAV) as well as for uninterruptible power supply (UPS) inverters.
Based on the new micro-pattern trench technology, the EconoDUAL 3 with the TRENCHSTOP IGBT7 chip performs with much lower static losses compared to the modules with an IGBT4 chipset. Additionally, its on-state voltage is reduced by up to 30 percent for the same chip area. This brings significant loss reduction in applications, especially for industrial drives, which usually operate at moderate switching frequencies. The oscillation behavior and the controllability of the IGBT have been improved. Additionally, the new power modules feature a maximum overload junction temperature of 175°C.
The new chip dimensions enable optimization of the module layout to reduce switching losses. As a result, the switching losses for the 600 A module are reduced by up to 24 percent compared to the former generation. This leads in a simplified design-in for applications with higher switching frequency. Furthermore, all features can be implemented in the same footprint facilitating the upgrade of existing inverter system designs. With the extended 750 A and 900 A versions, the EconoDUAL 3 package addresses an improved inverter power range. In addition, the PressFIT housing enables a fast and cost-efficient assembly.
Availability
The 1200 V TRENCHSTOP IGBT7 EconoDUAL™ 3 portfolio can be ordered now. Variants with pre-applied TIM will also be available soon. More information is available at www.infineon.com/econodual3 and www.infineon.com/igbt7.
Learn about Infineon’s contribution to energy efficiency: www.infineon.com/green-energy.
Information Number
INFIPC202109-095
Press Photos
-
Based on the TRENCHSTOP™ IGBT7 chip, the EconoDUAL™ 3 performs with much lower static losses compared to the modules with an IGBT4 chipset. Additionally, its on-state voltage is reduced by up to 30 percent for the same chip area which brings significant loss reduction in the application – especially for industrial drives, which usually operate at moderate switching frequencies.EconoDUAL_3_TRENCHSTOP_IGBT7
JPG | 168 kb | 2126 x 1555 px