OPN Frequently Asked Questions
Why are the existing ordering codes not sufficient?
What is the structure of the OPN / how does the OPN look like?
How are these attributes encoded?
Since the designator is non-speaking, how can I see what is behind that OPN?
How can I find the difference between two products with differing identifiers?
What is the maximum length of the OPN?
What is the benefit of the OPN?
Does every product have an OPN?
Can the OPN be used instead of the SP#?
Can the OPN be used instead of the Salesname?
Does the regular label show the OPN?
Does the OPN replace any existing product name?
What do I need to do if I use the pCPN?
Is the information shown in the OPN true for samples?
Do Engineering Samples have an OPN?
Do Development Kits and Boards have an OPN?
Where do I get a translation table?